|
|
 |
RENESAS TOOL NEWS on February 1, 2006: RSO-E8_1-060201D
The E8 Emulator Software
Revised to V.2.06 Release 01 |
We have revised the software for the E8 on-chip debugging emulator from
V.2.06 Release 00 to V.2.06 Release 01
- Descriptions of Revision
| 1.1 |
|
The Emulator Debuggers Revised
Three of the emulator debuggers included with the emulator software have
been revised at the same time. The revised debuggers are as follows:
- R8C/Tiny E8 emulator debugger V.2.02.01
- M16C/Tiny, M16C/62P E8 emulator debugger V.1.02.01
- M32C/80 E8 emulator debugger V.1.01.01
Note that the H8/300H Tiny, H8/300H Super Low Power, H8/300L Super Low
Power E8 emulator debugger V.1.01.01 remains as before (not revised).
|
| 1.2 |
|
A Problem Fixed in Emulator Debuggers
The following problem has been fixed: The Interrupt Enable flag
(the I flag) is not set to 1 when single-step execution performed in
the interrupt handling function has allowed processing to return
from the interrupt routine serviced to the main program.
The H8/300H Tiny, H8/300H Super Low Power, H8/300L Super Low Power
E8 emulator debugger is not involved in this problem.
|
| 1.3 |
|
The Evaluation Version of the M3T-NC30WA C-Compiler Package Revised
The evaluation version of the M3T-NC30WA C-compiler package included
with the emulator software has been revised from V.5.40 Release 00
to V.5.40 Release 00A. For details of the revision, see RENESAS TOOL
NEWS No. RSO-M3T-NC30WA-060201D, published on February 1, 2006. |
- Restriction
When the H8/38327F or H8/38347F MCU is targeted for debugging,
using the LCD or WDT Reset function may result in the Communication
Timeout Error.
For details, see RENESAS TOOL NEWS No. RSO-E8_2-060201D,
published on February 1, 2006.
- How to Update Your Product
Free-of-charge update is available. If you are using the software
product, download the executable file of the update program from Download
site and execute it.
NOTICES:
- You can select the update program out of two, the full-package and
the light version. The former contains a full set of the emulator
debuggers for the E8 emulator, the High-performance Embedded
Workshop, the evaluation version of the C compiler package, the
AutoUpdate utility, and the user's manual. Note, if you select the
latter, that it contains the emulator debuggers for the E8 emulator
and the High-performance Embedded Workshop only.
- If the update program is executed in the system where the High-
performance Embedded Workshop V.4.00.02 or earlier resides, it will
be upgraded to V.4.00.03.
|
 |