Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 1, 2006: RSO-HI7000/4-060201D

Notes on Using the Real-Time OS HI7000/4

Please take note of the following problems in using the real-time OS HI7000/4, which supports the SuperH RISC engine family of MCUs evolved from the SH-1, SH-2, SH2-DSP, SH-2E (excluding FPU version), SH-2A, and SH2A-FPU cores:
  • On using SH-1-cored MCUs
  • On using sample programs


  1. Problem on Using SH-1-Cored MCUs
    1.1   Versions Concerned
    HI7000/4 V.2.01 Release 00--V.2.02 Release 01

    1.2   Description
    If a service call that handles variable-size memory pools is made by using the new method* of managing them in any SH-1-cored MCU, a general invalid instruction exception may happen in the kernel, which prevents the system from operating normally.
    * To use this new method, open the Modification of Variable-Size Memory Pool Information dialog box in the configurator, and check the new method [CFG_NEWMPL] check box. For details of the new method, see the "Variable-Size Memory Pool" section in the user's manual.

    1.3   Workaround
    Don't use the new method of managing variable-size memory pools; that is, don't check the CFG_NEWMPL check box.

    1.4   Schedule of Fixing the Problem
    We have no plan to fix this problem. It is a restriction imposed on all the SH-1-cored MCUs.


  2. Problem on Using Sample Programs
    2.1   Versions Concerned
    HI7000/4 V.2.02 Release 00 and later

    2.2   Description
    A unified sample program "kernel_exp.src" (interrupt and exception processing routines) has been included with the HI7000/4 V.2.02 Release 00 and later instead of the previous two files of "nnnn_expent.src" and "nnnn_intdwn.src".
    So use "kernel_exp.src" in the HI7000/4 V.2.02 Release 00 or later.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal