Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
Download Site of An MCU file and an IO file
for Compact Emulator R0E436640CPE00
for the H8/300H Tiny Series MCUs


  1. Download
    Please download the following installer to install an MCU file and an IO file that are required when you use R0E436640CPE00 on H8/36049 group MCUs.

    ContentsFile name 
    Installer of
    MCU file and IO file
    for H8/36049 group MCUs
    MCUIO_Files_install_cpe_h8tiny_060512.exe Download
    (EXE 76.0 KB)

    We have revised the above installer on May 22, 2006.

    Note:
    New MCU file is updated on March 20, 2007. Refer to here.

  2. How to Use the download file
    Invoke the downloaded installer.
    Following the guidance, execute the installer to add and update an MCU file and an IO file for H8/36049 group to your emulator debugger.


  3. Note
    You must connect a converter board R0E436049CFJ10 for H8/36049 group to your emulator R0E436640CPE00 in addition to the above installation. Please confirm whether a R0E436049CFJ10 is connected to R0E436640CPE00 before using R0E436640CPE00.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal