Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on February 16, 2006: RSO-R0E436640CPE00SR_2-060216D

A Note on Using
the H8/300H Tiny Compact Emulator Debugger V.1.00 Release 00

Please take note of the following problem in using the emulator debugger V.1.00 Release 00 for the R0E436640CPE00 compact emulator (the emulator is used for the H8/300H Tiny series of MCUs):
  • On downloading object files created by the compiler package for the H8SX, H8S, and H8 families


  1. Description
    When you download object files created by the compiler package for the H8SX, H8S, and H8 families into the emulator, an error may arise, resulting in none of the files being downloaded. At this time, the following error message will appear:

    Failed to get the DW_AT code in the offset [0xXXXXXX]
    (at=0x2a, form=0x6)(1552)


  2. Solution
    This problem has been resolved in the revised product--the emulator debugger V.1.01 Release 00.
    So please download its installer from HERE and install it.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal