|
|
 |
RENESAS TOOL NEWS on March 1, 2006: RSO-R0E436049CFJ10-060301D
A Converter Board
for the H8/300H Tiny Series Compact Emulator R0E436640CPE00 Released |
We have released a converter board--R0E436049CFJ10--for the H8/300H Tiny series compact emulator R0E436640CPE00. This board is used for connecting the emulator with the 80-pin 0.65-mm-pitch QFP package (the package for the H8/36049 MCU group).
- Outline
The R0E436049CFJ10, which is used together with the H8/300H Tiny series compact emulator R0E436640CPE00, enables you to connect the emulator with the 80-pin 0.65-mm-pitch QFP package (PRQP0080JB-A*) in the user system in order to emulate members of the H8/36049 MCU group.
Note that you need the MCU and the I/O file for those MCUs to emulate them using the R0E436640CPE00 compact emulator. For how to introduce the MCU and I/O file, see Section 3 below.
* The previous code names are FP-80A and FP-80AV.
For details of the specifications of the converter board, see its datasheets.
- The Contents of the Product Package
| (1) |
|
A converter board--R0E436049CFJ10--for the H8/36049 group
- A slave board--R0E436049EPBS0--for the H8/36049 group
- A converter board--R0E436049CFJ10--for connecting the 80-pin 0.65-mm-pitch QFP package
- A 150-mm FFC cable
|
| (2) |
|
An 80-pin 0.65-mm-pitch IC socket--IC149-080-017-B5--manufactured by Yamaichi Electronics Co., Ltd. |
| (3) |
|
A user's manual |
- How to Introduce the MCU and the I/O File for the H8/36049 Group
The MCU and the I/O file needed to emulate members of the H8/36049 group using the R0E436640CPE00 compact emulator can be introduced as follows:
| (1) |
|
Download the installer program
"MCUIO_Files_install_cpe_h8tiny_060202.exe" for introducing the MCU and the I/O file for the H8/36049 group from HERE. |
| (2) |
|
Execute the installer to save the MCU and the I/O file into your emulator debugger.
|
- Ordering Information
If you place an order for the product, please supply the following items of information to your local Renesas Technology sales office or distributor:
| (1) |
|
Converter board R0E436049CFJ10 only
| Product type |
R0E436049CFJ10 |
| Type Name |
R0E436049CFJ10 |
|
| (2) |
|
Suit package R0E436049CPE10
This package comprises the converter board R0E436049CFJ10 and the compact emulator R0E436640CPE00
| Product type |
R0E436049CPE10 |
| Type Name |
R0E436049CPE10 |
|
For the prices contact your local Renesas Technology sales office or distributor.
|
 |