|
|
 |
RENESAS TOOL NEWS on March 1, 2006: RSO-E200F-060301D
The Emulator Software for the E200F Emulator R0E0200F1EMU00
Revised to V.2.01 Release 00 |
We have revised the emulator software for the E200F emulator R0E0200F1EMU00 from V.2.00 Release 00 to V.2.01 Release 00. This software is used to emulate the SH-2- and SH-2A-cored MCUs, SuperH RISC engine family.
- Versions to Be Revised
The emulator software V.1.00 Release 00--V.2.00 Release 00
for the R0E0200F1EMU00 emulator, which is used to emulate the SH-2- and SH-2A-cored MCUs, SuperH RISC engine family.
- Description of Revision
All the devices in the following groups have been supported:
| Groups |
Series |
| SH7083, SH7084, SH7085, and SH7086 |
SH7080 |
| SH7124 and SH7125 |
SH7125 (SH/Tiny) |
| SH7146 and SH7149 |
SH7146 |
| SH7147 |
SH7147 |
| SH7211 |
SH7210 |
- How to Update Your Product
Free-of-charge online update is available. If you are using the product concerned, go through the following steps:
| (1) |
|
Download the update program of the product from Download site. |
| (2) |
|
Decompress the downloaded ZIP file to obtain the install program (a setup.exe file); then execute it. |
- Notice
If the install program is executed in the system where the High- performance Embedded Workshop V.4.00.02 or earlier resides, it will be upgraded to V.4.00.03.
|
 |