|
|
 |
RENESAS TOOL NEWS on March 16, 2006: RSO-E10A-USB-060316D
A Note on Using
the Emulator Software Packages
for the E10A-USB Emulators
and an E200F Emulator |
Please take note of the following problem in using the emulator software
packages for the E10A-USB emulators and an E200F emulator, which are used
for emulating the SuperH RISC engine family of MCUs:
- On erroneous descriptions in the I/O file for the SH7211F MCU, SH7211
group, SH7210 series
- Products and Versions Concerned
- Emulator software V.2.03 Release 00
for the E10A-USB emulators (HS0005KCU01H and HS0005KCU02H)
- Emulator software V.2.01 Release 00
for the E200F emulator (R0E0200F1EMU00)
- Descriptions
Erroneous descriptions have been found in the I/O file for the SH7211F
(the SH7211.io file), which is included in the products concerned.
Since they cause errors to arise in the I/O Register window, please
rectify them as follows:
| (1) |
|
[UBC]
Delete the following four items:
BDR_0
BDMR_0
BDR_1
BDMR_1 |
| (2) |
|
[Compare_Match_Timer]
Replace the six items shown in the 1st raw of the following table
with the corresponding ones in the 2nd raw:
-------------------------------
CMCSR0 CMCSR_0
CMCNT0 CMCNT_0
CMCOR0 CMCOR_0
CMCSR1 CMCSR_1
CMCNT1 CMCNT_1
CMCOR1 CMCOR_1 |
| (3) |
|
[Serial_Communication_Interface_with_FIF02]
Add the following item:
SCSEMR_2 |
| (4) |
|
[A/D Converter]
Replace the addresses of the 17 registers shown in the 2nd raw of
the following table with the corresponding ones in the 3rd raw:
Register Address Address
------------------------------------------
ADCR0 0xFFFFE400 0xFFFFE800
ADSR0 0xFFFFE402 0xFFFFE802
ADICER0 0xFFFFE404 0xFFFFE804
ADIEFR0 0xFFFFE406 0xFFFFE806
ADISR0 0xFFFFE408 0xFFFFE808
ADISTR0 0xFFFFE40A 0xFFFFE80A
ADIEIER0 0xFFFFE40C 0xFFFFE80C
ADSTRGR0 0xFFFFE41C 0xFFFFE81C
ADANSR0 0xFFFFE420 0xFFFFE820
ADDR0 0xFFFFE440 0xFFFFE840
ADDR1 0xFFFFE442 0xFFFFE802
ADDR2 0xFFFFE444 0xFFFFE804
ADDR3 0xFFFFE446 0xFFFFE806
ADDR4 0xFFFFE448 0xFFFFE808
ADDR5 0xFFFFE44A 0xFFFFE80A
ADDR6 0xFFFFE44C 0xFFFFE80C
ADDR7 0xFFFFE44E 0xFFFFE80E
Also delete the following two items:
ADCR1
ADSR1 |
| (5) |
|
[Pin_Function_Controller]
Replace the address of the register shown in the 2nd raw of
the following table with the corresponding one in the 3rd raw:
Register Address Address
------------------------------------------
IFCR 0xFFFE3A22 0xFFFE38A2 |
- Workaround
To circumvent this problem, follow these steps:
| (1) |
|
Download the corrected I/O file for the SH7211F (SH7211.io) (File size: 3.15 KB). |
| (2) |
|
Then overwrite the previous SH7211.io file with the corrected one.
The I/O file is saved in the IO Files folder, which is under the
directory where any of the products concerned is installed. |
- Schedule of Fixing the Problem
We plan to fix this problem in the next release of the products.
|
 |