|
|
 |
MESC TOOL NEWS:
MESCT-PDB30-971116D
PDB30, PDB30SIM
Precaution
|
Please care about the problem described bellow which occurs in using M16C/60 series debuggers PDB30 and PDB30SIM (for Windows).
Products and Versions Concerned
This problem occurs in the following products and versions:
- all versions of PDB30
- all versions of PDB30SIM
Problem
The absolute module file (X30 file) that is produced using linker ln30 with
command parameters over 255 characters cannot correctly be loaded with a
format error.
Solution
When command parameters exceeding 255 characters are needed, please use a
command file. A command file is a one in which command parameters are
described. By informing ln30 of a command file name, command parameters
are read from the file.
[Example of command file]
File name "cmdfile"
sample1 sample2 sample3 . . . . -ORDER ram=80 -ORDER prog, sub, data -M
|
[Specifying command file]
ln30 @cmdfile
(A command file is specified by adding an "at" mark (@) at the beginning
of the file name.)
|
For details of ln30 command files, refer to "ln30 command option (@)" in
"AS30 User's Manual, ".
Revision Schedule
This problem is to be cleared up in the next upgraded version.
|
 |