Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESC-M16C-980316D

Remodeling of the Emulation Pods
for M16C/60 and 61 into the one for M16C/62

Mitsubishi is going to accommodate your request to remodel the emulation pods for the M16C/60 and 61 groups of microcomputers into the one for the M16C/62 group with additional charge, from Apr. 1, 1998.
Please apply for the remodeling of your emulation pod if you approve the limitations imposed on using the remodeled pods. A detailed explanation of these limitations is given below.



Limitations Imposed on Using Remodeled Pods
The remodeling of emulation pods comes with the following limitations.

  1. When your emulation pod for the M16C/60 or 61 is remodeled into the one for the M16C/62 group, the pod becomes dedicated to debug the M16C/62 group; not available for debugging the M16C/60 or 61 group.

  2. Maximum operating frequencies are limited to the values shown in Table 1.

    Table 1. Maximum Operating Frequencies (After Remodeling)
    Operating VoltageMaximum Operating Frequency
    5.0 Vat 0 WAIT10.0 MHz
    at 1 WAIT16.0 MHz
    3.0 Vat 1 WAIT7.0 MHz


  3. Remodeled pods cannot be used for debugging in Memory Space Expansion Modes 1 and 2.

  4. Pull-up control registers

    When Reset is removed with the CNVss pin tied to Vcc, the pull-up resistors connected to P45-P47 go to the OFF state.

  5. Port control register function of the port P1

    Regardless of the setting of the port control register, the port P1 reads an input level as a input port, and reads contents of the port P1 register as an output port.

  6. Emulator debuggers used with remodeled pods

    1. PDB30 V.2.00 Release 2 or older
      Usable as it is

    2. PD30 V.3.00 or later
      Select "M30600.MCU" as "MCU" in the Init dialog box which appears after starting PD30.
      (PD30 does not operate correctly if "M30620.MCU" is selected.)

    [Application effective]
    From Apr. 1, 1998 to Dec. 25, 1998 inclusive
    After the above date application will not be acceptable.

    [Ordering Information]
    1. Remodeling the emulation pod for the M16C/60 group into the one for the M16C/62 group:
    • Type Name: MSCH-TOOL-H-PD
    • Comment: M30600T-RPD M16C/62 Remodel
    2. Remodeling the emulation pod for the M16C/61 group into the one for the M16C/62 group:
    • Type Name: MSCH-TOOL-H-PD
    • Comment: M30610T-RPD M16C/62 Remodel

    [Send to]
    Your local Renesas Technology sales office or distributor

    [Notes]
    1. If your emulation pod does not operate normally, the extra charge for repairing it will be added.
    2. In the above case, we will not be able to replace the defective pod with a new one.
    3. Remodeling takes more than 2 weeks from receiving your pod to shipping it.
    4. If the M30600T-RPD-E and M30610T-RPD-E emulation pods (overseas versions) are remodeled, they lose the capability for use in overseas.

    For technical inquiries about the remodeling, contact your local Renesas Technology sales office or distributor.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal