|
|
 |
MESC TOOL NEWS:
MESCT-PC4701-980401D
Tools for Supporting 7515 and 3850/3851 Groups
|
Mitsubishi announces that the tool sets for the 7515 and 3850/3851 groups of the 740 family microcomputers have been modified as it has developed the new emulator MCUs for those groups.
MCUs
M37516RSS for 7515 group
M37517RSS for 3850/3851 group
Tool Sets
| Group | Previous Set | Modified Set |
| 7515 | PC4701 system + M37515T-RPD* | PC4701 system + M38000TL2-FPD + M37516RSS |
| 3850/3851 | PC4701 system + M37515T-RPD* | PC4701 system + M38000TL2-FPD + M37517RSS |
* Note that the production of M37515T-RPD is terminated as the tool sets have been modified.
Conversion Boards
The following conversion boards are provided for modified tool sets:
- For M37516RSS (targeted to 48-pin QFP foot pattern)
| Product Name | Type Name | Comment |
| 64DIP-DMS | MSCH-TOOL-H-ZZ | 64DIP-DMS |
| M37515T-PTC | MSCH-TOOL-H-ZZ | M37515T-PTC |
- For M38517RSS (targeted to 42-pin SSOP foot pattern)
| Product Name | Type Name | Comment |
| 42DIP-DMS | MSCH-TOOL-H-ZZ | 42DIP-DMS |
| DIRECT42-450-50 | MSCH-TOOL-H-ZZ | DIRECT42-450-50 |
*28DP-WS is included with M38000TL2-FPD.
MCU Files
Corresponding to the modification explained above, it is necessary to rewrite MCU files. Please type "M38000.MCU" as the firmware file name for both of the modified tool sets.
| Tool Set | MCU File Name | Pod No.in MCU File |
| PC4701 system + M37515T-RPD | M37515.MCU | 40 |
| PC4701 system + M37516RSS or M38517RSS | M38000.MCU | 0 |
For MCU files and the description of the files, refer to manuals on emulator debuggers.
For technical inquiries, contact your local Renesas Technology sales office or distributor.
|
 |