|
|
 |
MESC TOOL NEWS:
MESCT-NC77WA-980516D
RASM77/NC77WA Upgraded Versions announcements
|
Mitsubishi announces that relocatable assembler RASM77 and C compiler NC77WA (including assembler and Integrated Tool Manager (TM)) for the 7700 family of microcomputers have been upgraded to the following:
- RASM77 V.5.00 Release 1
- NC77WA V.5.00 Release 1
Descriptions
- Supporting TM (Integrated Tool Manager)
NC77WA V.5.00 supports TM, which controls cross tools with graphical user interfaces (GUI) and provides integrated program development environment.
- C Compiler: NC77WA
- Command option -Wall has been added.
- The following problems have been fixed.
- Assembler: RASM77
- The precedence of searching for include files has been altered.
- The following problems have been fixed.
- Problem in using a '~' operator to an immediate value when '.DATA8' is given.
- Problem in making entries of 128 or more modules in LIB77
- Operating Environment
Windows NT 4.0 is supported.
- Publishing Media
All the products of the PC versions of RASM77 and NC77WA will be published in CD-ROMs.
Publishing Information
Owing to this upgrading, the publishing of the NC77 C compiler only is replaced by that of the upgraded NC77WA compiler, so that NC77WA will be supplied if NC77 is ordered. The upgrade from RASM77 to NC77WA is also accepted. Accordingly, the upgrading of NC77 only hereafter covers that of RASM77 without upgrading NC77 and RASM77 independently.
Ordering Information
Type names and comments required to order are shown below:
- Type Names
MSCH-TOOL-S-CC: new ordering of NC77WA
MSCH-TOOL-S-AS: new ordering of RASM77
MSCH-TOOL-S-VU: upgrading of your current version
- Comments
[Product Name + Supplement]-[Host Designation]-[Serial No. and License ID]
| | |
| | |
| | You are requested
| | to fill in at upgrading.
| |
| W95E: IBM PC/AT or compatible running Windows 95
| or Windows NT 4.0
|
NC77WA: new ordering of NC77WA
NC77WAVUP: upgrading of NC77WA
NC77WAGUP: upgrading of NC77 to NC77WA
RASM77: new ordering of RASM77
RASM77VUP: upgrading of RASM77
RASM77GUP: upgrading of RASM77 to NC77WA
- Example
Example of upgrading the Windows version of RASM77 to the one of NC77WA
Type Name: MSCH-TOOL-S-VU
Comments: RASM77GUP-W95E-Serial No.
|
 |