|
|
 |
MESC TOOL NEWS:
MESCT-PD16-980601D
PD16 V.1.20 Release 1 Upgraded Version Announcement
|
Mitsubishi announces that emulator debugger PD16 for the M16 family of microcomputers has been upgraded to PD16 V.1.20 Release 1.
Product Summary
PD16 V.1.20 Release 1 is an emulator debugger that controls emulators PC4901HS, PC4901L, PC4900H, and PC4900L for the M16 family of microcomputers.
Descriptions of Upgrading
The previous version (PDB16 V.1.10 Release 1) has been upgraded as follows:
- Extended Functions
- Supporting communications with LAN
LAN has been added to the communications interface with PC4901HS/PC4901L.
- Supporting long file names
Long file names can be used to save and download files.
- Modified functions
The following functions have been modified to remove each problem they come with:
- C watch window and local window
Problem: In the C watch and local windows, data is represented in 32 bits wide when there is no value within a range where variables of type signed char can be shown with characters.
- Calculation dialog box
Problem: If a calculation with the calculation dialog box indicates an abnormal result (representing "?????"), the radix is changed at the timing independent of user's intention.
- Hardware watch points
Problem: When the RAM monitor and hardware watch points are used, setting hardware watch points out of the range of RAM monitoring causes the following problems:
- Byte: Data is fixed to 01
- Half word: Uppermost 1 byte of data is fixed to 02
- Word: Uppermost 1 byte of data is fixed to 04
Host System Requirements
PD16 V.1.20 Release1 is hosted on an IBM PC/AT or compatible computer running Windows 95. Table 1 shows the host system requirements of PD16 V.1.20 Release1.
Table 1. Host System Requirements
| Computer | IBM PC/AT or compatible |
| OS | Windows 95 (*1) |
| CPU | i486 or higher (Pentium running at 75 MHz or higher recommended) |
| RAM Size (Including OS) | 8 MB or more (16 MB or more recommended) |
| Vacant Space of Hard Disk | 10 MB or more |
| Display | VGA or higher (1024 x 768 or more recommended) |
*1. When you use Microsoft Plus! for Windows 95 or Internet Explorer 4.0 or later (Active Desktop), PD16 might not operate correctly.
- If using Microsoft Plus!, uncheck the following check boxes:
[Property of Display], [Plus Tab], and [Drag as Window Contents Displayed]
- If using Active Desktop, uncheck the following check boxes:
[Property of Display], [Web Tab], [Folder Option], [Display], and [Drag as Window Contents Displayed]
Publishing Media
Hereafter the product is published in a CD-R, and the ID number that is inscribed in your license ID certificate is needed to install the software.
Ordering Information
Type names and comments required to order products are shown below. For inquiries on ordering, contact your local Renesas Technology sales office or distributor.
- Type Names
MSCT-TOOL-S-ED: For first ordering PD16
MSCT-TOOL-S-VU: For upgrading PDB16 V1.10 R1 to PD16
MSCT-TOOL-S-ZZ: For first ordering user's manual
- Comments for Products
[Product Name + Supplement]-[Host Designation]-[Serial No.]
| | |
| | |
| | Please fill in at upgrading.
| |
| W95E: for Windows 95
|
PD16: For first ordering PD16
PD16VUP: For upgrading PD16
- Comments for User's Manual
[Product Name]-[Language Designation]
| |
| |
| E: User's manual in English
|
PD16
- Example of Ordering
The type name and comments, for example, for upgrading PDB16 V.1.10 Release 1 to PD16 V.1.20 Release 1 are as follows:
Type Name: MSCT-TOOL-S-VU
Comments: PD16VUP-W95E-Serial No.
|
 |