|
|
 |
MESC TOOL NEWS:
MESCT-NC30WA_1-980801D
NC30WA V.3.00 Release 2 Upgraded Version Announcement
|
This is to announce that C compiler NC30WA V.3.00 Release 1 (with assembler and integrated tool manager) for the M16C/60 series of microcomputers has been upgraded to its V.3.00 Release 2.
Descriptions of Upgrading
The following problems have been fixed:
- Problem with 4-bit data transfer
For details refer to Tool News "NC30WA V.3.00 Release 1 Precaution" on June 1, 1998.
- Problem with divide operations
For details refer to Tool News "NC30WA V.2.00 Release 1, V.3.00 Release 1 Precaution" on July 1, 1998.
- Problem with stack information for bcopy function
For details refer to Tool News "NC30WA V.2.00 Release 1, V.3.00 Release 1 Precaution" on July 1, 1998.
- Problem with stk30 utility program
For details refer to Tool News "NC30WA V3.00 Release 1, AS30 V.3.00 Release 1 Precaution" on April 1, 1998.
- Problem with make.exe file in TM environment
For details refer to Tool News "NC30WA V.3.00 Release 1, NC77WA V.5.00 Release 1 Precaution" on June 16, 1998.
- Problem with environment variables of cross tools in using TM
For details refer to the Release Note of NC30WA V.3.00 Release 1.
How To Upgrade
Please download the upgraded version at our download site (to be opened from Sept. 1, 1998).
|
 |