Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-CC16-981001D

CC16 Precaution

Please take note of the following problem in using C compiler cc16 included in cross tool kit CC16 for the M16 family of microcomputers.


Versions Concerned
All the versions of cc16 are affected. The version number of your product can be examined by giving cc16 the starting option "-V".


Problem: Local Arrays Referenced Incorrectly
  1. Description
    If all of the following four conditions are satisfied, local arrays are referenced incorrectly.

  2. Conditions
    1. An option or options including optimization level 4 (-O4, -O5, -O6, -O7, -O, -Otime only, and -Ospace only) are given at compilation.
      Note: The options listed above are all including optimization level 4.
    2. An array defined as a local variable exists in statements.
    3. A function call exists in statements, and the address of the local array in condition 2 is passed to the argument of the function.
    4. After the function call in condition 3, the local array in condition 2 is referenced more than once.

  3. Example
    ----------------------------------------------------------------------
    
       extern void foo2( int * ); 
       extern int x;
       extern int y;
       void foo( void )
       {   
          int     mx[1];          /* condition (2) */
          foo2( &mx[0] );         /* condition (3) */
          x = mx[0];              /* condition (4) */
          y = mx[0];              /* condition (4) */
       }
    
    ----------------------------------------------------------------------
    
  4. Workaround
    Circumvent this problem by using any one of the following four ways:
    1. Not to give any option including optimization level 4 at compilation

    2. To declare the array in condition 2 above to be volatile
      --------------------------------------------------------------------
        
          extern void foo2( volatile int * ); /* declared to be volatile */
          extern int x;
          extern int y;
          void foo( void )
          {   
             volatile int     mx[1];         /* declared to be volatile */
             foo2( &mx[0] );
             x = mx[0];
             y = mx[0];
          }   
        
      --------------------------------------------------------------------
      
    3. To define the array in condition 2 above as a global variable.
      --------------------------------------------------------------------
        
          extern void foo2( int * );
          extern int x;
          extern int y;
          int     mx[1];     /* defined as a global variable */
          void foo( void )
          {   
             foo2( &mx[0] );
             x = mx[0];
             y = mx[0];
          }
        
      --------------------------------------------------------------------
      
    4. To provide a pointer variable to reference local arrays
      --------------------------------------------------------------------
        
          extern void foo2( int * );
          extern int x;
          extern int y;
          void foo( void )
          {   
             int     mx[1];
             int     *mp = mx;       /* provides a pointer variable */
             foo2( mp );             /* uses the pointer variable */
             x = *mp;                /* uses the pointer variable */
             y = *mp;                /* uses the pointer variable */
          }   
        
      --------------------------------------------------------------------
      




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal