Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TOOL-981101D

Information on Windows 98 Hosted
Mitsubishi Development Support Tools

This is to inform you that our latest development support tools can be hosted on Windows 98 as well.


Products Involved
The latest versions of the following development support tools for Windows 95 also run properly on Windows 98.
  1. Cross tools
    SRA74, RASM77, NC77WA, AS79, NC79WA, AS30, NC30WA, CC32R

  2. Real-time OSs
    MR30K, MR30S, MR32RK, MR32RS

  3. Debuggers
    PD45, PD38, PD77, PDB77, PD77SIM, PD30, PD30SIM


Notes
  1. All the limitations imposed on the above mentioned products for Windows 95 are also encountered when the products run on Windows 98. For those limitations refer to the manual or release note of each product.
  2. The following debuggers can run on Windows 98 only when used with the serial or dedicated parallel interface (with the LAN interface they may not work well though this matter is under investigation):

    PD38, PD77, PD30




© 2003-2010 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap