|
|
 |
MESC TOOL NEWS:
MESCT-SRA74-981201D
Please take note of the following problems in using assembler SRA74 for the 740 family of microcomputers.
On Deleting Temporary Files
- Version Concerned
SRA74 V.2.00 Release 2 for Windows 95
- Problem
When debug source line information is produced in SRA74 for Windows 95, temporary files will not automatically be deleted. This problem occurs if either of the following two conditions is satisfied:
- The "-C" option is used.
- The ".FUNC" pseudo instruction exists in the source file.
- Workaround
When debug source line information is produced using thr "-C" option or others, please delete temporary files manually.
On Character Strings Generated by Pseudo Instruction ".ERROR"
- Versions Concerned
All the versions of SRA74
- Problem
When the "-." option used, character strings will not be displayed on screen by the ".ERROR" pseudo instruction.
- Workaround
Don't use the "-." option in order to display character strings on screen by the ".ERROR" pseudo instruction.
- Schedule of Fixing Problems
We plan to fix these problems in our next release.
|
 |