|
|
 |
MESC TOOL NEWS:
MESCT-PD38SIM-981216D
New Product PD38SIM V.1.00 Release 1 Announcement
|
This is to announce the issuance of new Windows-hosted simulator debugger PD38SIM V.1.00 Release 1 for the 740 family of microcomputers.
Outline of Product
PD38SIM V.1.00 Release 1 (hereafter called PD38SIM) is a simulator debugger running on Windows for simulating the operation of the 740 family MCUs and evaluating the target systems based on them.
Features
PD38SIM provides the following features:
- Multiple Windows of Overlaid Type Supported
The overlaid multiple windows allow you to view a variety of information at one time.
- I/O Simulation Function
I/O functions of timers and others can be simulated using the I/O window and I/O script function.
- RAM Monitoring Function
The RAM monitoring function is supported to reference the contents of RAM while executing the target program.
- Customize Function
The user can set their own customized functions (custom commands and windows) to PD38SIM.
Ordering Information
| Computer | OS | Type Name | Comments |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-PD38SIM | W95E |
On User's Manual
The user's manual of PD38SIM is included in the electronic manual of the product in PDF. A paperbound version of the user's manual is also available with additional charge (the contents of it is the same as the electronic manual). If you need it, please place an order with the following type name and comments filled in:
- Type Name
- MESH-TOOL-S
- Comments
- PD38SIM-UE
|
 |