Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-SRA74_1-990116D

SRA74 V.4.00 Release 1
Upgraded Version Announcement

This is to announce that assembler SRA74 for the 740 family of microcomputers has been upgraded to its V.4.00 Release 1.


Descriptions of Upgrading

  1. TM (Integrated Tool Manager) Supported
    SRA74 V.4.00 is the product's first version of supporting TM, which controls cross tools using GUI and provides you with integrated program development environment.

  2. Functions Upgraded
    1. Expanded memory of the M37280 MCU for use in TV is supported.
    2. 32-bit signed integers are used as data in evaluating operational expressions.
    3. All the operands of expanded codes, which are long branches in structured description, are created as labels.
    4. The following problems have been fixed:

  3. Publishing Media
    CD-ROM or CD-R

  4. Miscellaneous
    This version can run on Windows NT 4.0 and Windows 98.
    The IBE version will be unified into W95E version after this upgrade.

Ordering Information
ComputerOS Type NameComments
IBM PC/AT or compatible Windows 98
Windows 95
Windows NT 4.0
M-SRA74 For first ordering: W95E
For upgrading: W95E-VUP-Serial No.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal