Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-NC79WA-990316D

NC79WA V.3.10 Release 1
AS79 V.3.10 Release 1
Upgraded Versions Announcement

This is to announce that C compiler (with assembler and integrated development environment) NC79WA and assembler AS79 for the 7900 series of microcomputers have been upgraded.


Descriptions of Upgrading
  1. C Compiler NC79
    (1) The following options have been introduced:
    • -fuse_DIV
      creates operations of type int = type long/int by div instructions
    • -finfo
      creates files of the information of variables needed by the DPnDATA declaration utility
    • -Wmake_tagfile
      outputs error and warning messages for each source file
    (2) The DPnDATA declaration utility supported.
    (3) Assembler macro functions supported.
    (4) All of the problems notified on our tool news have been fixed.
    (For details refer to 79xx Series Tool News)

  2. Assembler AS79
    (1) The following problems have been fixed:
    A macro local label is not correctly defined when the label is described immediately after a binary operator placed after a decimal value in a macro definition.
    (For details refer to Tool News No. 3 on October 16, 1998.)
    (2) Errors occur when the operand of MOVxxx instructions is not described within a single line.

  3. Load Module Converter lmc79
    (1) Machine language files created by lmc79 can be rearranged to be output in the ascending order of addresses.

  4. Absolute Lister abs79
    (1) The following problem has been fixed: in description lines using assembler directive ".ALIGN", placing whitespaces before and after a comma that delimits character strings may result in errors.
    (For details refer to Tool News No. 5 on December 1, 1998.)

  5. Cross Referencer xrf79
    (1) The maximum number of files that can be processed at a time has been extended up to 600.

  6. Integrated Development Environment TM
    (1) Projects can be produced by using real-time OS.
    (2) The launching of debuggers enables download to be performed, as well as parameters to be set.
    (3) When creating a Makefile the following customization functions are available:
    • Building configurators of the load module converter and real-time OS and batch files produced by the user.
    • Selecting an option for each source file.
    (4) Projects can be produced in existing directories.
    (5) Tree windows and output windows can be docked and/or floated.

Upgrade Service Information
  1. Online Upgrading
    Please download the upgraded product from HERE.

  2. Upgrading in CD-ROM
    The upgrading by CD-ROM is also available with additional charge. For inquiries on upgrade service, please contact your local Renesas Technology sales office or distributor.

    Ordering Information
    ComputerOSType NameComments
    IBM PC/AT or compatibleWindows 98
    Windows 95
    Windows NT 4.0
    M-NC79WA
    or
    M-AS79
    For first ordering:W95E
    For upgrading:W95E-VUP-Serial No.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal