|
|
 |
MESC TOOL NEWS:
MESCT-NC77WA-990316D
NC77WA V.5.10 Release 1 Upgraded Version Announcement
|
This is to announce that C compiler (with assembler and integrated development environment) NC77WA for the 77XX series of microcomputers has been upgraded.
Descriptions of Upgrading
Outlines of upgrading are as follows:
- C Compiler NC77
(1) Option "-Wmake_tagfile" (-WMT) has been introduced. Error messages generated in each file are written into an error file created for each file.
(2) Options "-O [1--5]" have been introduced to facilitate the selection of an optimizing option.
(3) The following problems notified on our tool news have been fixed:
- Integrated Development Environment TM
(1) Projects can be produced by using real-time OS.
(2) The launching of debuggers enables download to be performed, as well as parameters to be set.
(3) When creating a Makefile the following customization functions are available:
- Building configurators of the load module converter and real-time OS and batch files produced by the user.
- Selecting an option for each source file.
(4) Projects can be produced in existing directories.
(5) Tree windows and output windows can be docked and/or floated.
Upgrade Service Information
- Online Upgrading
Please download the upgraded product from HERE.
- Upgrading in CD-ROM
The upgrading by CD-ROM is also available with additional charge. For inquiries on upgrade service, please contact your local Renesas Technology sales office or distributor.
Ordering Information
| Computer | OS | Type Name | Comments |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-NC77WA |
For first ordering:W95E For upgrading:W95E-VUP |
|
 |