|
|
 |
MESC TOOL NEWS:
MESCT-PD38-990408D
PD38 V.3.00 Release 1A Upgraded Version Announcement
|
This is to announce that emulator debugger PD38 for the 740 family of microcomputers has been upgraded to V.3.00 Release 1.
Descriptions
PD38 V.3.00 Release 1 is an emulator debugger for the 740 family of 8-bit microcomputers. Hosted on a PC running Windows, it controls the operation of the PC4701 emulator (PC4701M/PC4701HS/PC4701L) to debug application programs and target systems.
It has been upgraded from its preceding version, PD38 V.2.00 Release 1, as follows:
Functions Extended
The functions explained below have been introduced to the upgraded version.
- Supporting new emulator PC4701M
- Functions added on Program and Source Windows
- By placing the mouse cursor on a C variable for a fixed time, the value of the variable is displayed on the popup window.
- Results of coverage measurement can be displayed.
- Right-clicking the mouse allows the user to jump to selected functions or make entries of selected variables in the C-watch window.
- Functions added on C-Watch Window
- The values of variables can be displayed during execution of the target program by using the information of the RAM monitor function.
- The elements of an array and the contents a pointer points to can be displayed.
- A RADIX can be modified for each variable.
- Functions added on Trace Window
- Execution history can be recorded up to 32K cycles.
- Trace measurement can be forced to stop during execution of the target program to reference the results of tracing. The trace measurement forced to stop can be resumed.
- The execution time for each instruction is displayed in DIS and SRC display modes.
Problems Fixed
The following problems encountered in the preceding PD38 V.2.00 Release 1 have been fixed:
- When executing the G command (in the earlier command system), the target program cannot be stopped at any break address if the instruction at the address is 2 bytes long or more.
[ For details refer to Tool News No. 4 on June 16, 1998. ]
- In M37531, M37532, M37536, and M37630 MCUs, the firmware file included with PD38 V.2.00 Release 1 cannot be used.
[ For details refer to Tool News No. 1 on June 1, 1998. ]
- Information at storing data and one at reading the data differ each other in the following two items of information:
- Information on hardware breakpoints in the hardware breakpoint setting dialog box
- Information on trace points in the trace point setting dialog box (for emulators PC4701HS and PC4700H only)
[ For details refer to Tool News No. 6 on December 1, 1998. ]
Upgrade Service Information
Either of the following two methods of upgrading is available according to the version of the customer's product:
- The customer who has their license ID : Choose online upgrading or upgrading by CD-ROM
- The customer who has their serial number : Select upgrading by CD-ROM. Please ensure the serial number of your product is filled in after VUP in the comments.
[ Example ]:W95E-VUP-Serial No.
- Online upgrading (without charge)
Please download the upgraded product from HERE.
- Upgrading by CD-ROM (with additional charge)
The upgrade service is available in CD-ROM with additional charge. For further information, please contact your local Renesas Technology sales office or distributor.
Ordering Information
| Computer | OS | Type Name | Comments |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 |
M-PD38 | For first ordering:W95E For upgrading:W95E-VUP |
- On User's Manual
The user's manual of PD38 is included in the electronic manual of the product in PDF. The paperbound version of the user's manual is also available with additional charge (the contents of it is the same as the electronic manual). If you need it, please place an order with the following type name and comments filled in:
- Type Name........ MESH-TOOL-S
- Comments.......... PD38-UE
|
 |