Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PD79SIM-990401D

PD79SIM V.2.00 Release 1
Precaution

Please take note of the following problem in using simulator debugger PD79SIM (Windows version) for the 7900 series of microcomputers.


Description
PD79SIM does not support real-time OS MR79 V.2.00 Release 1 for the 7900 series of 16-bit microcomputers published on April 1, 1999. Note that, accordingly, when target programs created with the above-mentioned version of MR79 are debugged by PD79SIM, the following debug functions cannot be used:
  1. MR window
  2. MR commands

However, debug functions for the real-time OS can be used when target programs created with the following versions of MR79 are debugged:
  1. MR79 V.1.00 Release 1
  2. MR79 V.1.10 Release 1
Schedule of Fixing Problem
We plan to support MR79 V.2.00 Release 1 in our next release.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal