Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PD79-990401D

PD79 V.2.00 Release 1
Upgraded Version Announcement

This is to announce that emulator debugger PD79 for the 7900 series of microcomputers has been upgraded to V.2.00 Release 1.


Descriptions
PD79 V.2.00 Release 1 is an emulator debugger for the 7900 series of 16-bit microcomputers. Hosted on a PC running Windows, it controls the operation of the PC4701 emulator (PC4701M/PC4701HS/PC4701L) to debug application programs and target systems.It has been upgraded from its preceding version, PD79 V.1.10 Release 1, as follows:

Functions Extended
The functions explained below have been introduced to the upgraded version.

  1. Supporting new emulator PC4701M

  2. Functions added on Program and Source Windows
    • By placing the mouse cursor on a C variable for a fixed time, the value of the variable is displayed on the popup window.
    • Results of coverage measurement can be displayed.
    • Right-clicking the mouse allows the user to jump to selected functions or make entries of selected variables in the C-watch window.

  3. Functions added on C-Watch Window
    • The values of variables can be displayed during execution of the target program by using the information of the RAM monitor function.
    • The elements of an array and the objects of a pointer can be displayed.
    • A RADIX can be modified for each variable.

  4. Functions added on Trace Window
    • Execution history can be recorded up to 32K cycles.
    • Trace measurement can be forced to stop during execution of the target program to reference the results of tracing. The trace measurement forced to stop can be resumed.
    • The execution time for each instruction is displayed in DIS and SRC display modes.
Problem Fixed
The following problem encountered in the preceding PD79 V.1.10 Release 1 has been fixed:

  • The MW command issued for the contents of memory at an even address will not change the upper 8 bits of them.
    (For details refer to Tool News No. 2 on March 1, 1999.)

Upgrade Service Information
  1. Online upgrading (without charge)
    Please download the upgraded product from HERE.

  2. Upgrading by CD-ROM (with additional charge)
    The upgrade service is available in CD-ROM with additional charge. For further information, please contact your local Renesas Technology sales office or distributor.

    Upgrade Service Information
    ComputerOSType NameComments
    IBM PC/AT or compatible Windows 98
    Windows 95
    Windows NT 4.0
    M-PD79For first ordering:W95E
    For upgrading:W95E-VUP


  3. On User's Manual
    The user's manual of PD79 is included in the electronic manual of the product in PDF. The paperbound version of the user's manual is also available with additional charge (the contents of it is the same as the electronic manual). If you need it, please place an order with the following type name and comments filled in:

    • Type Name......... MESH-TOOL-S
    • Comments........... PD79-UE




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal