|
|
 |
MESC TOOL NEWS:
MESCT-MM-990501D
MM V.2.00.10 Upgraded Version Announcement
|
This is to announce that mask file utility MM has been upgraded to MM V.2.00.1.0.
Description of Upgrading
- The following problem has been fixed:
If the filename extension of a mask file is typed in uppercase (.MSK) in order to check the settings of the file, the file cannot be found.
- The English version is available from this upgrade on.
Upgrade Service Information
Please download the upgraded product from HERE.
Host System Requirements
| Computer | OS |
| IBM PC/AT or Compatible | Windows 98 Windows 95 Windows NT 4.0 |
|
 |