|
|
 |
MESC TOOL NEWS:
MESCT-PD30-990501D
PD30 V.4.00 Release 1
PD79 V.2.00 Release 1
PD77 V.2.00 Release 1
Precautions
|
Please take note of the following problem in using simulator debugger PD30 for the M16C/60 and M16C/20 series, emulator debugger PD79 for the 7900 series, and emulator debugger PD77 for the 77XX series of microcomputers.
Condition Involved
The problem occurs under the condition that any of the emulator debuggers shown below is used together with any of emulators PC4701M, PC4701HS, and PC4700H.
- PD30 V.4.00 Release 1
- PD79 V.2.00 Release 1
- PD77 V.2.00 Release 1
Description
Script commands HardwareBreak (HB) and TracePoint (TP) may not correctly be executed in the following format:
--------------------------------------------------------------------------
|
| >HB An, address, access condition, comparison data[:valid bit],
| comparison condition
| >TP Bn, address, access condition, comparison data[:valid bit],
| comparison condition
|
--------------------------------------------------------------------------
* The items enclosed within [ ] can be omitted.
[Example of Input]
--------------------------------------------------------------------------
|
| >HB A1, 400, WRITE, 5:7, !=
| >TP B2, 410, READ, 10, >
|
--------------------------------------------------------------------------
Workaround
This problem will be circumvented by using custom commands m_hb and m_tp that have been prepared to allow the HB and TP commands to be executed correctly. Also, the hardware breakpoint and trace point setting dialog boxes can set events normally. For information on installing and using the custom commands, refer to the README file included in the hb_e.exe file to be supplied.
How To Get the hb_e.exe File
Download the file (137KB) from here .
|
 |