Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PC4701HS-990601D

PC4701HS Self-Check
Precaution

Please take note of the following problem in using emulator PC4701HS for the M16C, 7700, and 740 families of microcomputers.


Products Concerned
ProductSerial No.
PC4701HS Emulator Unit9EE1913F or later (indicating the lots fabricated in or after May 1999)


Problem
If a PC4701HS emulator and an emulator debugger are used in their combination described below, performing self-check may result in incorrect termination. Combination of emulator and emulator debugger:

    Emulator:
    A PC4701HS product of the lots fabricated in and after May 1999
    Emulator Debugger:
    A PD30, PD38, PD77, or PD79 product of the earlier versions than the one upgraded in April 1999

Note:
All the products of PC4701 fabricated in and before April 1999 (with serial number 9DE1912E or earlier) are not concerned with this problem.

Solution
This problem will be eliminated by using the latest version of the emulator debuggers published in April 1999.
The latest version of each emulator debugger is as follows:

About ProductsComponent Support
Product NameVersionThe day of Release
PD30V.4.00 Release 1Apr. 1, 1999M16C/60 and M16C/20 series MCUs
PD79V.2.00 Release 1 Apr. 1, 19997900 series MCUs
PD77V.2.00 Release 1Apr. 1, 19997700 and 7751 series MCUs
PD38V.3.00 Release 1AApr. 8, 1999740 series MCUs


Upgrade Service Information
Product NameURL Address TO BE Referred To
PD30 PD30 V.4.00 Release 1 Upgraded Version Announcement on Apr. 1, 1999
PD79 PD79 V.2.00 Release 1 Upgraded Version Announcement on Apr. 1, 1999
PD77 PD77 V.2.00 Release 1 Upgraded Version Announcement on Apr. 1, 1999
PD38 PD38 V.3.00 Release 1A Upgraded Version Announcement on Apr. 8, 1999





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal