|
|
 |
MESC TOOL NEWS:
MESCT-PD308SIM-990616D
PD308SIM, PD30, PD30SIM, PD79, and PD79SIM
Precautions
|
Please take note of the following problem in using debuggers PD308SIM for the M16C/80 series, PD30 and PD30SIM for the M16C/60 and M16C/20 series, and PD79 and PD79SIM for the 7900 series of microcomputers.
Products Concerned
All the versions of the following products are concerned with this problem:
| Products Name | Description |
| PD308SIM | Simulator debugger for M16C/80 series MCUs |
| PD30 | Emulator debugger for M16C/60 and M16C/20 series MCUs |
| PD30SIM | Simulator debugger for M16C/60 and M16C/20 series MCUs |
| PD79 | Emulator debugger for 7900 series MCUs |
| PD79SIM | Simulator debugger for 7900 series MCUs |
Problem
Absolute module files with greater than 127 sections will not be downloaded by a debugger fault.
Workaround
If the number of sections in a program is greater than 127, download the file through the following procedure:
- After creating an absolute module file, produce a machine language file (an Intel HEX file or a Motorola S-format file) by using the load module or HEX file converter included in the compiler.
- Download the machine language file produced in step 1 by selecting the [File] -> [Download] -> [Memory Image...] command from the PDxx menu bar.
- Then, download the symbol information of the absolute module file by selecting the [File] -> [Download] -> [Symbol...] command.
Schedule of Fixing Problem
We plan to fix this problem in our next release.
|
 |