Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-TM-990716D

TM V.2.01 Upgraded Version Announcement

This is to announce that the Integrated Development Environment (TM) bundled with compilers and assemblers has been upgraded to its Version 2.01.


  1. Descriptions of Upgrading

    1.1 Supporting CC32R
    TM is enhanced to support CC32R on the occasion of CC32R's upgrade.

    1.2 High-Speed Opening of Project Files
    As the number of project files to be entered continues increasing, the capability of reading these files has been much improved.


  2. How To Upgrade TM

    2.1 Online upgrading (without charge)
    Please download the upgraded product from HERE.

    Note:
    Both of CC32R and TW32R were upgraded this time as well as TM. Every customer who has purchased or upgraded either of them need not upgrade their TM because TM V.2.01 is bundled with the purchased or upgraded product. Customers using TM V.2.00 or earlier in combination with NC308WA, NC30WA, NC79WA, NC77WA, or SRA74 are encouraged to online-upgrade their TM.





© 2003-2009 Renesas Technology Corp., All rights reserved. Web Site Usage Conditions| Privacy| Sitemap