Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-SRA74-990801D

SRA74 V.4.00 Release 1 Precaution

Please take note of the following problem in using assembler SRA74 for the 740 family of microcomputers.


  1. Description
    An erratum is found in the release note of SRA74 V.4.00 Release 1.


  2. Whereabouts
    In the descriptions of upgrading from the previous version on page 4


    [Right]
    In SRA74 V.4.00.00 or later, expressions are evaluated as of type 32-bit signed integer. However, only the following three values are treated as such in the results of evaluating the expressions.

    • An operand of the ".ORG" directive
    • An operand of the ".IF" directive <-------------------------- To be added
    • The value of a label when the "-BANK" option is used.


    [Wrong]
    In SRA74 V.4.00.00 or later, expressions are evaluated as of type 32-bit signed integer. However, only the following two values are treated as such in the results of evaluating the expressions.

    • An operand of the ".ORG" directive
    • The value of a label when the "-BANK" option is used.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal