Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-MR32R_1-990816D

MR32R V.3.10 Release 1
Upgraded Version Announcement

This is to announce that the products of real-time OS MR32R for the M32R family of microcomputers have been upgraded to the following versions:
Real-Time OS Development Kit: MR32RK V.3.10 Release 1
Real-Time OS Mass Production Contract: MR32RS V.3.10 Release 1


  1. Descriptions of Upgrading

    1.1 All of the problems known have been eliminated.
    For these problems, refer to the MR32R Precautions announced on and after April 16, 1999.

    1.2 Task trace, system call trace, and system call issue functions have been implemented.
    Note that these functions can be used by the emulator available and emulator/simulator debuggers to be released provided that those tools are capable of supporting them.

    1.3 The scheduler has been relocated to another section, so that it can operate on high-speed memory.

    1.4 Automatic timer setup function supports a lot of MCUs.


  2. How to Upgrade Current Products and Order Upgraded Ones
    MR32R is a product for a special user. If you need the latest version of Real-time OS with online, please ask csc@renesas.com.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal