Announcement of Opening Download Site for SRA74 Manuals
This is to announce the opening of the download site for manuals of the SRA74 assembler for the 740 family of microcomputers.
URL of Download Site for SRA74 Manuals
Please download from HERE.
To Customers of SRA74 V.4.00 Release 1
The manual of SRA74 V.4.00 Release 1 in PDF cannot be viewed correctly on the OS as a result of some imperfections contained in it. You are kindly requested to download the new PDF files corresponding to the following ones at the above download site:
These are manuals of freeware programs included in SRA74 V.4.00 Release 1.