|
|
 |
MESC TOOL NEWS:
MESCT-PD308-991016D
PD308 V.1.00 Release 1 Precaution
|
Please take note of the following problem in using emulator debugger PD308 for the M16C/80 series of microcomputers.
- Problem
If 1 KB or more of memory contents are transferred by using the MOVE command in the script window, a communication error may occur, resulting in PD308 being terminated.
- Workaround
If transfer of memory is performed by using the MOVE command, configure the addresses of the transfer source in such a way that the memory size transferred at one time is 400 H bytes or less.
- Schedule of Fixing Problem
We plan to fix this problem in our next release on November 1.
|
 |