Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-PD32RSIM-991101D

New Product
PD32RSIM V.1.00 Release 1
Announcement

This is to announce the issuance of simulator debugger PD32RSIM V.1.00 Release 1 for the M32R family of microcomputers.


  1. Outline of Product
    PD32RSIM V.1.00 Release 1 (hereafter called PD32RSIM) is a Windows-hosted simulator debugger that simulates operations of the Mitsubishi M32R family of 32-bit MCUs and evaluates their target systems. For further information on the product, refer to here.

  2. Ordering Information
    The type name and comment required to order PD32RSIM are shown below. For inquiries on ordering, contact your local Renesas Technology sales office or distributor.
    ComputerOSType NameComment
    IBM PC/AT or compatible Windows 98
    Windows 95
    Windows NT 4.0
    M-PD32RSIM For first ordering :W95E


  3. On User's Manual
    The user's manual of PD32RSIM is included in the electronic manual of the product in PDF. The paperbound version of the user's manual is also available with additional charge (the contents of it is the same as the electronic manual). If you need it, please place an order with the following type name and comment filled in:

    Type Name : MESH-TOOL-S
    Comment : PD32RSIM-UE




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal