|
|
 |
MESC TOOL NEWS:
MESCT-PD308-991101D
PD308 V.1.10 Release 1, PD30 V.4.10 Release 1
PD79 V.2.10 Release 1, PD77 V.2.10 Release 1
and PD38 V.3.10 Release 1
Upgraded Versions Announcement
|
This is to announce that emulator debuggers PD308, PD30, PD79, PD77, and PD38 have been upgraded as follows:
| For the M16C/80 series MCUs | | PD308 V.1.10 Release 1 |
| For the M16C/60, M16C/20 series MCUs | | PD30 V.4.10 Release 1 |
| For the 7900 series MCUs | | PD79 V.2.10 Release 1 |
| For the 77XX series MCUs | | PD77 V.2.10 Release 1 |
| For the 740 family MCUs | | PD38 V.3.10 Release 1 |
The descriptions of upgrading were added. For details of the additional information, refer to MESC TOOL NEWS "Improved Speed Performances
of PD308, PD30, PD79, PD77 and PD38 Upgraded Versions (Downloading Speed etc.)" issued on November 16, 1999.
- Descriptions of Upgrading
- 1.1 Functions Extended
- (1)The addition of the NextHide check box to the EMEM dialog box enables you to omit the setting of this dialog box at the next launching (PD308 only).
- (2)The MR task pose window is available (PD308 only).
- (3)Access sizes and masking can be specified at the PID settings of the state transition break window and the state transition trace window (PD308 and PD30 only).
- (4)Write conditions can be saved simultaneously at the saving of trace information in the state transition trace window.
- (5)The WORD size can be used as an access size at the PID settings of the RTOS Information dialog box in the task trace window (excepting PD38).
- (6)The history of searches can be saved in the Find dialog box.
- (7)The Chip Break dialog box can reference and delete chip breakpoints (PD79 only).
- 1.2 Problems Fixed
- (1)All of the problems encountered in the preceding PD308 V.1.00 Release 1 have been fixed.
- [For details refer to every piece of Tool News describing "PD308 Precaution" issued after July 1, 1999 (release date of the preceding version).
- (2)All of the problems encountered in the preceding PD30 V.4.00 Release 1 have been fixed.
- [For details refer to every piece of Tool News describing "PD30 Precaution" issued after Apr. 1, 1999 (release date of the preceding version).
- (3)All of the problems encountered in the preceding PD79 V.2.00 Release 1 have been fixed.
- [For details refer to every piece of Tool News describing "PD79 Precaution" issued after Apr. 1, 1999 (release date of the preceding version).
- (4)All of the problems encountered in the preceding PD77 V.2.00 Release 1 have been fixed.
- [For details refer to every piece of Tool News describing "PD77 Precaution" issued after Apr. 1, 1999 (release date of the preceding version).
- (5)All of the problems encountered in the preceding PD38 V.3.00 Release 1A have been fixed.
- [For details refer to every piece of Tool News describing "PD38 Precaution" issued after Apr. 1, 1999 (release date of the preceding version).
- How To Upgrade Current Products and Order Upgraded Ones
- 2.1 Online upgrading (without charge)
- Please download each of the upgraded products from our tool homepage.
- 2.2 First ordering or upgrading by CD-ROM (with additional charge)
- The upgrade service is available in CD-ROM as before with additional charge. The type names and comments required to order the upgraded products are shown below. For inquiries on upgrading or ordering, contact your local Renesas Technology sales office or distributor.
| Computer | OS | Type Name | Comments |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-PD308 M-PD30 M-PD79 M-PD77 M-PD38 | For first ordering :W95E For upgrading:W95E-VUP-[Serial No.]
[Serial No.]: See Note |
Note: Type the serial number of your product if the product is independent of a license ID.
- 2.3 On User's Manual
- The user's manual of each of the products is included in the electronic manual of it in PDF. The paperbound version of the user's manual is also available with additional charge (the contents of it is the same as the electronic manual). If you need it, please place an order with the following type name and comments filled in:
-
| Type Name | : | MESH-TOOL-S |
| Comments | : | PD308-UE, |
| | : | PD30-UE, |
| | : | PD79-UE, |
| | : | PD77-UE, or |
| | : | PD38-UE, |
|
 |