Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-NC30WA-991101D

NC30WA V.3.20 Release 1
and
AS30 V.3.20 Release 1
Upgraded Versions Announcement

This is to announce that C compiler and relocatable assembler for the M16C/60 and M16C/20 series of microcomputers have been upgraded as follows:
  • C Compiler (with Assembler and Integrated Development Environment) :
         NC30WA V.3.20 Release 1
  • Relocatable Assembler:
         AS30 V.3.20 Release 1

  1. Descriptions of Upgrading
    1.1 C compiler NC30
    (1)Special page declaration utility SPUTL supported.
    (2)Option added to display warning message.
    (3)Optimization upgraded.
    (4)The known problems fixed.
    [For details refer to every piece of Tool News describing "NC30WA Precaution" issued after Mar. 16, 1999 (release date of the preceding version).

    1.2 Relocatable assembler AS30
    (1)Operations including character strings can be described in operands in assembler directive commands and mnemonics.
    (2)The known problems fixed.
    [For details refer to every piece of Tool News describing "AS30 Precaution" issued after Mar. 16, 1999 (release date of the preceding version).


  2. How To Upgrade Current Products and Order Upgraded Ones
    2.1 Online upgrading (without charge)
    Please download each of the upgraded products from our tool homepage.

    2.2 First ordering or upgrading by CD-ROM (with additional charge)
    The upgrade service is available in CD-ROM as before with additional charge. The type names and comments required to order the upgraded products are shown below. For inquiries on upgrading or ordering, contact your local Renesas Technology sales office or distributor.

    ComputerOSType NamesComments
    IBM PC/AT or compatible Windows 98
    Windows 95
    Windows NT 4.0
    M-NC30WA
    M-AS30
    For first ordering:W95E
    For upgrading:W95E-VUP-[Serial No.]

    Note: Type the serial number of your product if the product is independent of a license ID.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal