Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-M30620TB-RPD-E-991101D

M30620TB-RPD-E
Remodeling Announcement

This is to announce that we are going to remodel the specific products of emulation pod M30620TB-RPD-E for the M16C/62 group of microcomputers.


  1. Products Concerned
    Product NameDescriptions
    M30620TB-RPD-EEmulation Pod for M16C/62 group MCUs
    (Maximum operating frequency: 16.0 MHz, Operating voltages: 4.8 -- 5.2 V)
    Serial Nos. 9HS570H -- 9HS627H fabricated in Aug. 1999 (a total of 58 pieces)

    Note 1: M30620T-RPD-E and M30620T2-RPD-E not included
    Note 2: Serial Nos. are marked at the backside of pods


  2. Problem Involved
    When data is written to an address of the emulation memory in the pod, this data may also be written to another address.
    [Example]
     ------------------------------------------------------------------------
     (1)Before writing to RAM
                        0  1  2  3  4  5  6  7  8  9  A  B  C  D  E  F
                  1000 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
                  1010 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
                  1020 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
     
     (2)An instruction for writing FFh into address 1000 of RAM executed
     
     (3)After writing to RAM
                        0  1  2  3  4  5  6  7  8  9  A  B  C  D  E  F
                  1000 FF 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
                  1010 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
                  1020 FF 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
     
                  The same data is written to addresses 1000 and 1020.
     ------------------------------------------------------------------------
    
    Note: The reproducibility of the symptom varies with the environment the pod is used and variations in the characteristics of semiconductor devices.

  3. Cause of Malfunction
    Changing the type of the emulation memory device mounted in the pod has resulted in write timing errors. This change was made from the production lots of the pods in August 1999 on.

  4. Remodeling of Products
    We will remodel every product concerned without charge, so you are kindly requested to send back your emulation pod, if it involved, to your local Renesas Technology sales office or distributor.
    The remodeling takes the number of days shown below, so please send back your pod as early as possible. Note that we will not be able to replace your pod with a new one for its remodeling period.

    (1)Received from Nov. 1 to Dec. 15, 1999 : Shipped about 5 workdays after reception.
    (2)Received from Dec. 16 to Dec. 28, 1999 : Shipped in order of reception after Jan. 15, 2000.
    (3)Received after Jan. 5, 2000 : Shipped about 10 workdays after reception.

    Note:Transportation time isn't contained.

    Please send the pods to MESC via Mitsubishi Overseas Marketing-MCU & ASIC Semiconductor Group.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal