|
|
 |
MESC TOOL NEWS:
MESCT-NC77WA-991101D
NC77WA V.5.20 Release 1 and RASM77 V.5.10 Release 1 Upgraded Versions Announcement
|
This is to announce that C compiler and relocatable assembler for the 77xx series of microcomputers have been upgraded as follows:
- C Compiler (with Assembler and Integrated Development Environment) :
NC77WA V.5.20 Release 1
- Relocatable Assembler:
RASM77 V.5.10 Release 1
- Descriptions of Upgrading
- 1.1 NC77WA V.5.20 Release 1
-
- (1)Faster compilation.
- (2)An option added to give a warning that the upper portion of a longer-typed value is lost when it is assigned to a shorter-typed value, for instance.
- (3)An option added to give a warning that an auto variable with no value is used.
- (4)The known problems fixed.
- For details refer to every piece of Tool News describing "NC77WA Precaution" issued after Mar. 16, 1999 (release date of the preceding version), from
- NC308WA, NC30WA, NC79WA and NC77WA precautions [May 16,1999]
- NC77WA and NC77 Precautions [Jun. 16,1999]
- NC79WA, NC77WA Precautions [Aug. 1, 1999]
- NC79WA, NC77WA Precautions [Oct. 16, 1999]
- 1.2 RASM77 V.5.10 Release 1
- (1)The problem fixed which expands macro arguments described in the fault statements of conditional assembling.
- (2)Branch optimization tool br77 introduced as a freeware product.
- If the destination of a branch instruction is outside the addressable range, an assemble error occurs. Tool br77 can convert such an instruction to the one with which the branch is possible. Please download br77 from here.
- How To Upgrade Current Products and Order Upgraded Ones
- 2.1 Online upgrading (without charge)
- Please download each of the upgraded products from our tool homepage.
- 2.2 Upgrading by CD-ROM (with additional charge)
- The upgrade service is available in CD-ROM as before with additional charge. For inquiries on upgrading, contact your local Renesas Technology sales office or distributor.
The type names and comments required to order the upgraded products are shown below:
| Computer | OS | Type Names | Comments |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-NC77WA M-RASM77 | For first ordering:W95E For upgrading:W95E-VUP-[Serial No.] |
Note: Type the serial number of your product if the product is independent of a license ID.
|
 |