Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-MR308-991116D

MR308 V.1.00 Release 2
Upgraded Version Announcement

This is to announce that the products of real-time OS MR308 for the M16C/80 series of microcomputers have been upgraded to the following versions:
Real-Time OS Development Kit : MR308K V.1.00 Release 2
Real-Time OS Mass Production Contract : MR308S V.1.00 Release 2


  1. Descriptions of Upgrading
    (1)The following known problems fixed:
    The problem on using INT instructions to issue system calls [ For details refer to "MR308 V.1.00 Release 1 Precaution" issued on Oct. 1, 1999, ]
    The problem on "makefile" files created by configurator cfg308 (EWS version only) [ For details refer to "MR308, MR30 Precautions" issued on Sept. 1, 1999, ]

    (2)The type of PT_MSG changed when message size is 16 in the mail box function
    (3)Special page subroutine calls supported
    (4)The processings of the vrst_blk system call improved
    (5)Describing a system call of ret_int() inadvertently in a C program interpreted as an error at linking
    (6)The processing of the tslp_tsk system call with the timeout value set to 0 improved
    (7)The __SB__ symbol changed from the EQU symbol to the address symbol
    (8)The task pause function--a debugging function of PD308--supported
    (9)Data items used for debugging placed separately in the MR_RAM_DBG section


  2. How to Upgrade Current Products and Order Upgraded Ones
    MR308 is a product for a special user.
    If you need the latest version of Real-time OS with online, please ask csc@renesas.com.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal