|
|
 |
MESC TOOL NEWS:
MESCT-NC308WA-991216D
NC308WA V.2.00 Release 1 and
AS308 V.2.00 Release 1
Upgraded Versions Announcement
|
This is to announce that C compiler and relocatable assembler for the M16C/80 series of microcomputers have been upgraded as follows:
| * C Compiler (with Assembler and Integrated Development Environment) | NC308WA V.2.00 Release 1 |
| * Relocatable Assembler | AS308 V.2.00 Release 1 |
-
Descriptions of Upgrading
- 1.1 C compiler NC308
- (1)SBDATA declaration utility SB308 supported.
- (2)Special page declaration utility SP308 supported.
- (3)Optimizing options level-structured with new options added.
- (4)An option added to display a warning message.
- (5)Optimization upgraded.
- (6)The known problems fixed.[For details refer to every piece of Tool News describing "NC308WA Precaution" issued after Feb. 1, 1999 (release date of the preceding version).]
- 1.2 Relocatable assembler AS308
- (1)Even when operands of assembler directive commands and mnemonics contain character strings, it is allowed to describe operations of these operands.
- (2)The maximum number of files treated at a time by cross referencer xrf308 extended up to 600.
- (3)The known problems fixed.[For details refer to every piece of Tool News describing "AS308 Precaution" issued after Feb. 1, 1999 (release date of the preceding version),]
-
How To Upgrade Current Products and Order Upgraded Ones
- 2.1 Online upgrading (without charge)
- Please download each of the upgraded products from HERE.
- 2.2 First ordering or upgrading by CD-ROM (with additional charge)
- The upgrade service is available in CD-ROM as before with additional charge. The type names and comments required to order the upgraded products are shown below. For inquiries on upgrading or ordering, contact your local Renesas Technology sales office or distributor.
| * Type Name of C Compiler NC308WA | | : M-NC308WA |
| * Type Name of Assembler AS308 | | : M-AS308 |
| Computer | OS | Type Name | Comment |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-NC308WA M-AS308 | For first ordering: W95E For upgrading: W95E-VUP |
|
 |