Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
MESC TOOL NEWS: MESCT-NC79WA_1-991216D

NC79WA V.3.20 Release 1
and
AS79 V.3.20 Release 1
Upgraded Versions Announcement

This is to announce that C compiler and relocatable assembler for the 7900 series of microcomputers have been upgraded as follows:
* C Compiler (with Assembler and Integrated Development Environment)NC79WA V.3.20 Release 1
* Relocatable AssemblerAS79 V.3.20 Release 1


  1. Descriptions of Upgrading
    1.1 C compiler NC79
    (1)Option -fauto_128 [-fA1] added: this option extends the upper limit of stack frame size from 64 to 128 bytes.
    (2)Function-extending #pragma MX1FUNCTION added: this function creates code provided that the MX flag is set to 1 at the beginning and ending procedures of a function.
    (3)An option added to display a warning message.
    (4)The known problems fixed. [For details refer to every piece of Tool News describing "NC79WA Precaution" issued after Aug. 1, 1999 (release date of the preceding version).]

    1.2 Relocatable assembler AS79
    (1)Tool SC79 added: this tool converts assembly language programs created by assembler RASM77 for the 7700 family MCUs into those for the 7900 family MCUs.
    (2)The known problems fixed. [ For details refer to every piece of Tool News describing "AS79 Precaution" issued after Aug. 1, 1999 (release date of the preceding version).]


  2. How To Upgrade Current Products and Order Upgraded Ones
    2.1 Online upgrading (without charge)
    Please download each of the upgraded products from HERE.

    2.2 First ordering or upgrading by CD-ROM (with additional charge)
    The upgrade service is available in CD-ROM as before with additional charge. The type names and comments required to order the upgraded products are shown below. For inquiries on upgrading or ordering, contact your local Renesas Technology sales office or distributor.
    * Type Name of C Compiler NC79WA M-NC79WA
    * Type Name of Assembler AS79 M-AS79
    ComputerOSType NameComment
    IBM PC/AT or compatible Windows 98
    Windows 95
    Windows NT 4.0
    M-NC79WA
    M-AS79
    For first ordering: W95E
    For upgrading: W95E-VUP-[Serial No.]
    Note: Type the serial number of your product if the product is independent of a license ID.




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal