|
|
 |
MESC TOOL NEWS:
MESCT-SRA74-991216D
SRA74 V.4.00 Release 2
Upgraded Version Announcement
|
This is to announce that relocatable assembler SRA74 for the 740 family of microcomputers has been upgraded to its Version 4.00 Release 2.
-
Descriptions of Upgrading
(1)Supported by TM V.2.01.
(2)The macro arguments in the "false" statement of conditional assembly aren't expanded.
(3)The directory where assembly language files created by an "include" file are saved is changed from the directory selected by environment variable INC to the one where the "include" file exists.
(4)The "-!8" option introduced to the operation with "!" operators: this option makes the lower 8 bits obtained by truncation after the "!" operation to be the result of the operation.
-
How To Upgrade Current Product and Order Upgraded One
- 2.1 Online upgrading (without charge)
- Please download the upgraded product from HERE.
- 2.2 First ordering or upgrading by CD-ROM (with additional charge)
- The upgrade service is available in CD-ROM as before with additional charge. The type name and comment required to order the upgraded product are shown below. For inquiries on upgrading or ordering, contact your local Renesas Technology sales office or distributor.
| Computer | OS | Type Name | Comment |
| IBM PC/AT or compatible | Windows 98 Windows 95 Windows NT 4.0 | M-SRA74 | For first ordering: W95E For upgrading: W95E-VUP-[Serial No.] |
Note: Type the serial number of your product if the product is independent of a license ID.
|
 |