|
|
 |
Issue Time:
V.5.41 Release 01 |V.5.41 Release 00 |
V.5.40 Release 00 | V.5.20 Release 02 | V.5.20 Release 1 | V.5.10 Release 1 | V.5.00 Release 1 |
V.3.10 Release 3 | V.3.10 Release 2 | V.3.10 Release 1 | V.3.00 Release 1 |
V.2.00 Release 2 | V.2.00 Release 1 |
V.1.00 Release 1 |
The news that had been issued on and after release date of M3T-NC308WA V.5.41 Release 01
In addition refer to the following News about High-performance Embedded Workshop.
| Issue Date |
Title |
Description |
Status on the
Latest Version |
| Jul. 16, 2008 |
A Note on Using the C Compiler Packages for the M16C MCU Family
--With Initializing a Member of a Structure Using an Expression Containing the sizeof Operator-- |
(1) With initializing a member of a structure using an expression
containing the sizeof operator |
Not Fixed |
| Jul. 16, 2008 |
A Note on Using the C Compiler Packages for the M16C MCU Family
--With Building a Static Function Having a Static Variable within It-- |
(1) With building a static function having a static variable within it |
Not Fixed |
| Jun. 16, 2008 |
A Note on Using the C Compiler Packages for the M16C MCU Family
--With Comparing a Bit Field Variable with 1 or 0-- |
(1) With comparing a bit field variable with 1 or 0 |
Not Fixed |
| Jun. 16, 2008 |
A Note on Using the C Compiler Packages for the M16C MCU Family
--With Using a Volatile-Qualified Variable in the for or while Statement-- |
(1) With using a volatile-qualified variable in the for or while statement |
Not Fixed |
| Apr. 16, 2008 |
A Note on Using the C Compiler Packages
for the R32C/100 and the M32C Series of MCUs |
(1) With issuing preprocessing directive #pragma DMAC to extend the C compiler's functionality |
Not Fixed |
| Mar. 1, 2008 |
A Note on Using the C Compiler Packages for the M16C MCU Family |
(1) With using preprocess command #error |
Not Fixed |
| Dec. 1, 2007 |
A Note on Using the C Compiler Packages for the M16C Family of MCUs |
(1) If a write to and a read from a bit field are made before and after
calling a function respectively |
Fixed |
| Jul. 16, 2007 |
A Note on Using the C Compiler Packages for the M16C Family of MCUs |
(1) With Using Options to Optimize Jump Instructions at Linking |
Not Fixed |
| Mar. 16, 2007 |
A Note on Using the C Compiler Packages
--M3T-NC308WA and M3T-NC30WA--
for the M16C MCU Family |
(1) Note of the problem in using the C compiler
packages--M3T-NC308WA and M3T-NC30WA--for the M16C MCU family |
Not Fixed |
| Mar. 16, 2007 |
A Note on Using the C Compiler Package
--M3T-NC308WA--
for the M32C MCU Series |
(1) Note of the problem in using the C compiler
package--M3T-NC308WA--for the M32C MCU series |
Not Fixed |
| Feb. 16, 2007 |
A Note on Using the C Compiler Packages
for the M32C MCU Series |
(1) With using the startup file in C language |
Not Fixed |
| Feb. 16, 2007 |
A Note on Using the C Compiler Packages
for the M32C and the M16C MCU Series |
(1) With performing operations of constants only |
Fixed |
| Dec. 16, 2006 |
The C Compiler Package--M3T-NC308WA--for the M32C MCU Series Revised to V.5.41 Release 01 |
(1)V.5.41 Release 00 -> V.5.41 Release 01. |
-- |
The news that had been issued on and after release date of M3T-NC308WA V.5.41 Release 00
The news that had been issued on and after release date of M3T-NC308WA V.5.40 Release 00
The news that had been issued on and after release date of M3T-NC308WA V.5.20 Release 02
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Dec. 1, 2005 |
A Note on Using the C Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On using the "-JOPT" option at linking |
Fixed |
| Nov. 16, 2005 |
A Note on Using the C Compiler Package M3T-NC308WA |
(1) On performing a subtraction containing a constant as a subtrahend |
Fixed |
| Nov. 16, 2005 |
A Note on Using the C Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On incorrect description of do statements |
Fixed |
| Nov. 1, 2005 |
A Note on Using the C Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On placing functions in sections |
Not Fixed |
| Oct. 1, 2005 |
A Note on Using the C Compiler Package M3T-NC308WA |
(1) On compiling programs where the real-time OS M3T-MR308 used |
Fixed |
| Aug. 16, 2005 |
A Note on Using the C Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On machine-language files created by the load module converter (lmc308 or lmc30) with the "-F" option selected |
Fixed |
| Jul. 16, 2005 |
A Note on Using the C Compiler Packages M3T-NC308WA and M3T-NC30WA--On Using Optimizing Option "-OR" |
(1) On using optimizing option "-OR" |
Fixed |
| Jul. 16, 2005 |
A Note on Using the C Compiler Packages M3T-NC308WA and M3T-NC30WA--On Defining More Than One Void Function |
(1) On defining more than one void function |
Fixed |
| Jun. 1, 2005 |
A Note on Using the C Compiler Packages
M3T-NC308WA and M3T-NC30WA--On Using the labs and abs Functions-- |
(1) On using the labs and abs functions
|
Fixed |
| Jun. 1, 2005 |
A Note on Using C-Compiler Package M3T-NC308WA--On Referencing Array-Type Variables Qualified with "const" |
(1) On referencing array-type variables qualified with "const" |
Fixed |
| Jun. 1, 2005 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA--On Passing a Pointer or Address to a Function as an Argument |
(1) On passing a pointer or address to a function as an argument |
Fixed |
| Apr. 1, 2005 |
A Note on Using the M3T-NC308WA C-Compiler Package |
(1) On using if-else constructs |
Fixed |
| Mar. 1, 2005 |
Information on Renesas's Development Software Products Capable of Running on Windows XP Service Pack 2 |
-- |
-- |
| Mar. 1, 2005 |
Notes on Using C-Compiler Package M3T-NC308WA |
(1) On using assembler directive commands ".ID" and ".PROTECT"
(2) On using assembler options "-mode60" and "-mode60p" |
Fixed |
| Mar. 1, 2005 |
C Compiler Package M3T-NC308WA Revised to V.5.20 Release 02 |
(1) V.5.20 Release 1 -> V.5.20 Release 02 |
-- |
The news that had been issued on and after release date of M3T-NC308WA V.5.20 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Feb. 16, 2005 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On successive statements each of which contains an operation of multiplication, addition, or subtraction between a variable of type float and a floating constant |
Fixed |
| Feb. 1, 2005 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA--On Calling a Function Declared to Be typedef and Returning a Structure |
(1) On calling a function declared to be typedef and returning a structure |
Fixed |
| Feb. 1, 2005 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA--On Using the Tool for Enhancing the Scan All Dependencies Function |
(1) On using the tool for enhancing the Scan All Dependencies function |
Fixed |
| Dec. 16, 2004 |
A Note on Using the M3T-NC308WA and M3T-NC30WA C-Compiler Packages--On Using the -OFFTI Compile Option |
(1) On using the -Oforward_function_to_inline (-OFFTI) compile option |
Fixed |
| Dec. 16, 2004 |
A Note on Using the M3T-NC308WA and M3T-NC30WA C-Compiler Packages--On Evaluation of Members of a Structure in the Controlling Expression of an If Statement |
(1) On evaluation of members of a structure in the controlling expression of an if statement |
Fixed |
| Dec. 16, 2004 |
A Note on Using the M3T-NC308WA and M3T-NC30WA C-Compiler Packages--On Evaluation of Elements of an Array in the Controlling Expression of an If Statement |
(1) On evaluation of Elements of an Array in the controlling expression of an if statement |
Fixed |
| Dec. 1, 2004 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On using inline functions |
Fixed |
| Nov. 16, 2004 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On nesting inline functions |
Not Fixed |
| Oct. 1, 2004 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On an inline function that returns a value of type _Bool |
Fixed |
| Sep. 16, 2004 |
A Note on Using C Compiler Package M3T-NC308WA |
(1) On a multiplication between variables of type long long |
Fixed |
| Sep. 16, 2004 |
A Note on Using C Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On using the near or far qualifier |
Fixed |
| Sep. 1, 2004 |
A Note on Using C Compiler Packages M3T-NC308WA and M3T-NC30WA--On Reading Members of Bit Fields in an Array |
(1) On reading members of bit fields in an array |
Fixed |
| Aug. 1, 2004 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA--On Using Options for the SQMlint |
(1) On using options for the SQMlint (a MISRA C rule-checker) |
Fixed |
| Aug. 1, 2004 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA--On Typing Three or More Successive Question Marks |
(1) On Typing three or more successive question marks |
Fixed |
| July 16, 2004 |
A Note on Using C Compiler Packages M3T-NC308WA and M3T-NC30WA |
(1) On calling the same function in both cases where the controlling expression of an if statement is TRUE and FALSE |
Fixed |
| July 1, 2004 |
A Note on Using C Compiler Packages M3T-NC308WA, M3T-NC30WA, M3T-NC79WA and M3T-NC77WA |
(1) On converting integer constants |
Fixed |
| July 1, 2004 |
A Note on Using C Compiler Packages M3T-NC308WA V.5.20 Release 1 and M3T-NC30WA V.5.30 Release 1 |
(1) On selecting link option "-JOPT" |
Fixed |
| May 16, 2004 |
A Note on Using C-Compiler Packages M3T-NC308WA and M3T-NC30WA--On Debug Information |
(1) On debug information |
Fixed |
| Apr. 16, 2004 |
A Note on Using C-Compiler Package M3T-NC308WA |
(1) On a division or remainder operation including a variable or constant of type long long |
Fixed |
| Apr. 1, 2004 |
Simulator Debuggers Bundled with C Compilers and Assemblers for the 8-, 16-, and 32-Bit MCUs |
(1) M3T-PD308SIM bundled with M3T-NC308WA |
-- |
| Mar. 16, 2004 |
C Compiler M3T-NC308WA Upgraded to V.5.20 Release 1 |
(1) V.5.10 Release 1 -> V.5.20 Release 1 |
-- |
The news that had been issued on and after release date of M3T-NC308WA V.5.10 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Mar. 1, 2004 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA--On Referencing Members in a Union |
(1) On referencing members in a union |
Fixed |
| Mar. 1, 2004 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA--On Testing Equality/Inequality Between a Variable and a Constant |
(1) On testing equality/inequality between a variable of type signed or unsigned char and a constant |
Fixed |
| Jan. 16, 2004 |
A Note on Using C Compiler M3T-NC308WA |
(1) On casting an integer-type value to a pointer-type one |
Fixed |
| Jan. 16, 2004 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On defining array-type variables |
Fixed |
| Nov. 16, 2003 |
A Note on Using C compilers M3T-NC308WA and M3T-NC30WA |
(1) On function calls using the indirection operator |
Fixed |
| Nov. 16, 2003 |
A Note on Using C compilers M3T-NC308WA and M3T-NC30WA |
(1) On declaring parameters in function definitions |
Fixed |
| Nov. 16, 2003 |
A Note on Using C compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA; and Assemblers AS308, AS30, and AS79 |
(1) On linking relocatable module files with no sections |
Fixed |
| Oct. 16, 2003 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On the division and remainder operations between constants |
Fixed |
| Oct. 16, 2003 |
A Note on Using C Compiler M3T-NC308WA |
(1) On comparing a variable with another one or a constant of type signed char in a conditional expression |
Fixed |
| Sep. 16, 2003 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On using the link option "-U" |
Fixed |
| Aug. 16, 2003 |
A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA |
(1) On arguments of formatted input/output functions |
Fixed |
| Aug. 16, 2003 |
A Note on Using C Compiler M3T-NC308WA |
(1) On calling a function indirectly |
Fixed |
| July 16, 2003 |
Notes on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On using the -Ocompare_byte_to_word (-OCBTW) compile option (2) On the character string length of a variable which have functions as array elements |
Fixed |
| June 16, 2003 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On displaying the values of arguments passed to a function |
Fixed |
| June 1, 2003 |
A Note on Using C Compiler M3T-NC308WA |
(1) On arithmetic right shift of a variable of type long long |
Fixed |
| June 1, 2003 |
A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA |
(1) On defining structure-type arrays |
Fixed |
| May 16, 2003 |
A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA and M3T-NC77WA |
(1) On standard library functions atof and strtod |
Fixed |
| May 1, 2003 |
A Note on Using C Compilers and Assemblers M3T-NC308WA, M3T-NC30WA, AS308, and AS30 |
(1) On the "MOVA" and "PUSHA" mnemonic instructions |
Fixed |
| May 1, 2003 |
C Compiler M3T-NC308WA V.5.10 Release 1 Upgraded |
(1) V.5.00 Release 1 -> V.5.10 Release 1 |
-- |
The news that had been issued on and after release date of M3T-NC308WA V.5.00 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Apr. 1, 2003 |
A Note on Using C Compiler M3T-NC308WA |
(1) On calling a function in an if-else construct |
Fixed |
| Mar. 16, 2003 |
A Note on Using C Compiler M3T-NC308WA |
(1) On defining bit fields as of type unsigned long |
Fixed |
| Mar. 16, 2003 |
Notes on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On using the #pragma ADDRESS declaration (2) On using the #pragma ADDRESS declaration or the volatile qualifier for a variable to be assigned to another |
Fixed |
| Mar. 16, 2003 |
A Note on Using C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA and M3T-NC77WA |
(1) On the standard library function "sprintf" |
Fixed |
| Mar. 1, 2003 |
A Note on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On placing auto variables |
Fixed |
| Feb. 1, 2003 |
Notes on Using C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On hexadecimal escape sequences of string literals (2) On subtract operations of addresses (3) On conditional jumps in iteration control structures |
Fixed |
| Dec. 16, 2002 |
Notes on C Compiler M3T-NC308WA V.5.00 Release 1 |
(1) On locating variables qualified by the type qualifiers "near" and "far" (2) On renaming a rom or data section by the #pragma SECTION directive command |
Fixed |
| Dec. 16, 2002 |
Information on Releasing the Function-Enhancing Patch Tool for TM V.3.20 Included with the Windows' Versions of C Compilers M3T-CC32R, M3T-NC308WA, and M3T-NC30WA |
-- |
-- |
| Dec. 1, 2002 |
Notes on C compilers M3T-NC308WA and M3T-NC30WA |
(1) On placing a #pragma ASM--ENDASM block immediately after the definition of an inline function (2) On defining inline functions |
Fixed ((2): Not concerned) |
| Oct. 1, 2002 |
Notes on C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA |
(1) On a union declared to be an auto variable (2) On a switch statement (A) (3) On a switch statement (B) (4) On successively referencing the same variable in more than one if statement (5) On warning option -Wno_used_argument (6) On directive commands #pragma JSRA and #pragma JSRW |
Fixed |
| Sep. 16, 2002 |
A Note on C Compilers M3T-NC308WA V.5.00 Release 1 and M3T-NC30WA V.5.00 Release 1 |
(1) On describing an if or switch statement |
Fixed |
| Sep. 16, 2002 |
Notes on C Compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA; and Assemblers AS308, AS30, and AS79 |
(1) On using command option "-O" in the load-module converter (2) On an "IF-ELIF-ENDIF" construct in structured description |
Fixed |
| Sep. 1, 2002 |
Notes on C compiler M3T-NC308WA V.5.00 Release 1 |
(1) On bit fields in a structure declared using the volatile qualifier (2) On defining arrays with a list of about 6200 or more initializers (3) On interrupt handling functions (4) On using bit fields and _Bool type variables |
Fixed |
| Aug. 1, 2002 |
C Compiler M3T-NC308WA Upgraded to V.5.00 Release 1 |
(1) V.3.10 Release 3 -> V.5.00 Release 1 |
-- |
The news that had been issued on and after release date of M3T-NC308WA V.3.10 Release 3
| Issue Date |
Title |
Description |
Status on the Latest Version |
| June 16, 2002 |
A Note on C Compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA; and Assemblers AS308, AS30, and AS79 |
(1) On using macro directive command ."LOCAL" |
Fixed |
| June 16, 2002 |
A Note on C Compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA |
(1) On using standard function libraries scanf, fscanf, and sscanf |
Fixed |
| June 1, 2002 |
Notes on C Compilers M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA; and Assemblers AS308, AS30, and AS79 |
(1) On jump addresses in switch statements (2) On directive command ".ORG" |
Fixed |
| June 1, 2002 |
Notification of MITSUBISHI Development Support Tools Running on Windows XP |
(1) Notification of Mitsubishi development support tools running on Windows XP |
-- |
| May 1, 2002 |
Notes on C Compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA |
(1) On testing bit fields in an if construct (2) On conditional expressions containing a subtraction |
Fixed ((2): Not concerned) |
| Apr. 16, 2002 |
Notes on C Compilers M3T-NC308WA, M3T-NC30WA, and M3T-NC79WA |
(1) On function-extending directive command "@" for concatenating character strings (2) On the tag jump function |
Fixed |
| Mar. 1, 2002 |
A Note on C Compilers M3T-NC308WA and M3T-NC30WA |
(1) On switch-case statements |
Fixed |
| Feb. 1, 2002 |
Compiler M3T-NC308WA Upgraded to V.3.10 Release 3 |
(1) V.3.10 Release 2 -> V.3.10 Release 3 |
-- |
The news that had been issued on and after release date of NC308WA V.3.10 Release 2
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Jan. 16, 2002 |
Notes on M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, AS308, AS30, and AS79 |
(1) On directive command ".INCLUDE" (2) On MAX instructions generated with an unnecessary comma attached (3) On describing location symbol "$" |
Fixed ((3): Not concerned) |
| Nov. 16, 2001 |
(IMPORTANT) M3T-NC308WA and M3T-NC30WA Precautions |
This news describes how to use compilers correctly to develop your target programs. So, please don't neglect reading this to prevent your programs from involving serious errors. (1) On optimizing functions of the compilers |
Specification change |
| Nov. 16, 2001 |
M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA Precautions |
(1) On domain errors arising at calling the "pow" function out of the standard library (2) On incorrect optimization made in a loop containing a switch statement (3) On forced termination of compilation by describing update of a pointer variable within a loop |
Fixed |
| Oct. 1, 2001 |
M3T-NC308WA, M3T-NC30WA, M3T-NC79WA, and M3T-NC77WA Precautions |
(1) On setting initial values for arrays of integer types (2) On making a comparison (including an equality/inequality test) between floating-point numbers using an if statement |
Fixed |
| Sep. 16, 2001 |
NC308WA, NC30WA, AS308, and AS30 Precautions |
(1) On the function of optimizing branch instructions |
Fixed |
| July 1, 2001 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) Descriptions of inline assemble functions have been omitted in User's Manual and Release Note |
Revised |
| July 1, 2001 |
NC308WA and NC30WA Precautions |
(1) On assembler macro descriptions in C-language source files (2) On link command option "-LOC" |
Fixed |
| May 16, 2001 |
NC308WA V.3.10 Release 2 and NC30WA V.4.00 Release 2 Precautions |
(1) On calling inline functions out of other ones |
Fixed |
| Apr. 16, 2001 |
Information on Mitsubishi's Development Support Tools Running on Windows Me |
(1) Information on Mitsubishi's development support tools running on Windows Me |
-- |
| Apr. 16, 2001 |
NC308WA and NC30WA Precautions |
(1) On describing assignment expressions within iteration statements |
Fixed |
| Apr. 16, 2001 |
NC308WA V.3.10 Release 2 Upgraded Version Announcement |
(1) V.3.10 Release 1 -> V.3.10 Release 2 |
-- |
The news that had been issued on and after release date of NC308WA V.3.10 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Apr. 1, 2001 |
NC308WA and NC30WA Precautions |
(1) On assigning variables or immediate values to members of a structure |
Fixed |
| Feb. 16, 2001 |
NC308WA V.3.10 Release 1 Precaution |
(1) On testing bit fields in an array (2) On arithmetic and logical shift instructions |
Fixed |
| Feb. 16, 2001 |
NC308WA and NC30WA Precautions |
(1) On using immediate values |
Fixed |
| Feb. 16, 2001 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) On declaring type "enum" (2) On the function-extending #pragma STRUCT directive |
Fixed |
| Jan. 16, 2001 |
NC308WA Precaution |
(1) On bitwise exclusive OR operations (2) On "if" statements with expressions testing bit fields (3) On multiplications of long or unsigned long type expressions (4) On generating the MAX instruction |
Fixed |
| Dec. 16, 2000 |
NC308WA Precaution |
(1) On pointers pointing to functions (2) On using a structure as an actual argument to a function with varying numbers of arguments |
Fixed |
| Dec. 16, 2000 |
NC308WA V.3.10 Release 1 Upgraded Version Announcement |
(1) V.3.00 Release 1 -> V.3.10 Release 1 |
-- |
The news that had been issued on and after release date of NC308WA V.3.00 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Nov. 1, 2000 |
NC308WA, NC30WA, NC79WA, AS308, AS30, and AS79 Precautions |
(1) On concatenating strings in assemblers (AS308, AS30, and AS79) (2) On the order of searching include files in assemblers (AS308, AS30, and AS79) |
Fixed |
| Nov. 1, 2000 |
Information on Mitsubishi Development Support Tools Running on Windows 2000 |
(1) Information on Mitsubishi development support tools running on Windows 2000 |
-- |
| Oct. 1, 2000 |
NC308WA, NC30WA, NC79WA, AS308, AS30, and AS79 Precautions |
(1) On the total size of ROM displayed in linkers ln308, ln30, and ln79 |
Fixed |
| Oct. 1, 2000 |
NC308WA V.3.00 Release 1, NC30WA V.4.00 Release 1, and NC79WA V.4.00 Release 1 Precautions |
(1) Describing the condition expression that tests bit fields in an "if" statement may result in incorrect code being generated (2) Utilities utl308, utl30, and utl79 may unexpectedly terminate their processing |
Fixed |
| Sep. 1, 2000 |
NC308WA and AS308 Precautions |
(1) On assembler directive command ".BTEQU" (2) On bit operation instructions |
Fixed |
| Sep. 1, 2000 |
NC308WA V.3.00 Release 1 Upgraded Version Announcement |
(1) V.2.00 Release 2 -> V.3.00 Release 1 |
-- |
The news that had been issued on and after release date of NC308WA V.2.00 Release 2
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Aug. 1, 2000 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) Converting the type of floating-point constants to the unsigned long one may cause their values to become incorrect |
Fixed |
| July 16, 2000 |
NC308WA Precaution |
(1) On flipping bit fields of more than 1 bit wide (2) On corrections of and additions to user's manuals for assembler macros |
Fixed |
| July 16, 2000 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) Assigning the address of a function to a variable of type pointer to another function results in a System Error being generated if the types of both functions are different from each other (2) Folding floating-point constants may cause incorrect subtract operations to be performed (3) Folding constants of type unsigned long may cause incorrect divide and modulus operations to be performed |
Fixed |
| June 16, 2000 |
NC308WA and AS308 Precautions |
(1) On using options for protecting ROM in lmc308 (2) On addition in floating-point arithmetic (3) On initialization of stack pointers |
Fixed |
| May 1, 2000 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) If an optimize option is used, Windows' error message may appear |
Fixed |
| Apr. 1, 2000 |
EWS-Version C Compilers, Assemblers, and Real-Time OSes Precautions |
(1) On installing by root user |
Fixed |
| Mar. 1, 2000 |
AS308, AS30, and AS79 Precautions |
(1) Double-defined labels may not be interpreted as errors at linking |
Fixed |
| Feb. 16, 2000 |
NC308WA V.2.00 Release 2, NC30WA V.3.20 Release 2, NC79WA V.3.20 Release 2, and NC77WA V.5.20 Release 2 Upgraded Versions Announcement |
(1) V.2.00 Release 1 -> V.2.00 Release 2 |
-- |
The news that had been issued on and after release date of NC308WA V.2.00 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Feb. 1, 2000 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) On compiling programs containing variables that are declared to be "const" |
Fixed |
| Feb. 1, 2000 |
NC308WA Precaution |
(1) On generating unintended STZX instructions (2) Errors in descriptions of the BZEROL and BCOPYL macros in the startup routine (3) Error in user's manuals on how to describe assembler functions |
Fixed |
| Jan. 16, 2000 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) Initialization of external variables of type float or double |
Fixed |
| Dec. 16, 1999 |
AS308 and AS30 Precautions |
(1) On starting up the linker with a command file selected |
Fixed |
| Dec. 16, 1999 |
NC308WA V.2.00 Release 1 and AS308 V.2.00 Release 1 Upgraded Versions Announcement |
(1) V.1.00 Release 1 -> V.2.00 Release 1 |
-- |
The news that had been issued on and after release date of NC308WA V.1.00 Release 1
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Oct. 16, 1999 |
NC308WA V.1.00 Release 1 Precaution |
(1) On arithmetic operations of integer constants cast to pointers (2) On calculation of stack usage including standard function library |
Fixed |
| Oct. 1, 1999 |
NC308WA Precaution |
(1) Additional information of MESC Technical News No. M16C-37-9910 "Note on Using INT Instruction in M16C/80 Group MCUs" issued on October 1, 1999 |
-- |
| Oct. 1, 1999 |
NC308WA and NC30WA Precautions |
(1) When a conditional branch statement including a return statement with no return value is described in a function with a return value, . . . |
Fixed |
| Oct. 1, 1999 |
AS308 Precaution |
(1) On as308 (2) On ln308 |
Fixed |
| Sep. 16, 1999 |
NC308WA V.1.00 Release 1 Precaution |
(1) When a normal interrupt handling function declared with #pragma INTERRUPT (without switch /F) is described in the source file . . . |
Fixed |
| Sep. 16, 1999 |
AS308, AS30, and AS79 Precautions |
(1) When an absolute module file is generated by a source file in which no section is declared, . . . |
Fixed |
| June 16, 1999 |
NC308WA and NC30WA Precautions |
(1) On multiplication of variables of type "int" and type "pointer to int" (2) On compilation of switch -- case statements |
Fixed ((1): Not concerned) |
| June 16, 1999 |
AS308 and AS30 Precautions |
(1) When assemblers are launched with undefined local symbols described in the address portions of operands of local bit symbols and assembler option "-S" given, . . . |
Fixed |
| May 16, 1999 |
NC308WA, NC30WA, NC79WA, and NC77WA Precautions |
(1) On arrays of type far with initial values (2) On "sizeof" operator |
Fixed |
| Apr. 1, 1999 |
NC308WA V.1.00 Release 1, NC30WA V.3.10 Release 1 Precautions |
(1) On optimization of conditional branch of setting and clearing 1 bit after testing it |
Fixed |
| Apr. 1, 1999 |
NC308WA V.1.00 Release 1 Precaution |
(1) On functions taking structure or union as argument |
Fixed |
| Apr. 1, 1999 |
lmc308 Upgraded Version Announcement |
(1) V.1.00.02 |
-- |
| Feb. 16, 1999 |
AS308 Precaution |
(1) On using abs308 |
Fixed |
| Feb. 1, 1999 |
New Products NC308WA V.1.00 Release 1, AS308 V.1.00 Release 1 Announcement |
(1) V.1.00 Release 1 |
-- |
|
 |