|
|
 |
| Real-time OS - M3T-MR30/4, M3T-MR30 |
See FAQs (PDF file: 2.85MB) |
Issue Time:
V.4.00 Release 00| V.4.00 Release 01 |
V.3.30 Release 2 | V.3.30 Release 1 |
V.3.20 Release 1 |
V.3.10 Release 1 |
V.3.00 Release 1 |
The news that had been issued on and after release date of M3T-MR30/4 V.4.00 Release 01
The news that had been issued on and after release date of M3T-MR30/4 V.4.00 Release 00
| Issue Date |
Title |
Description |
Status on the Latest Version |
| Jun. 16, 2008 |
Notes on Using the Real-Time OSes--M3T-MR308/4 and M3T-MR30/4--for the M16C MCU Family |
(1)With using mailboxes with the TA_MPRI property (NOTE 1)
(2)With calculating stack usage |
Fixed |
| Oct. 1, 2007 |
Real-Time OS M3T-MR30/4 Supports an Additional MCU Series |
(1) Added the R8C/Tiny series of
MCUs to its support line. |
-- |
| Aug. 1, 2007 |
Notes on Using the MR Series of Real-Time OSes |
(1) With using a set_flg or iset_flg service call in combination with
ichg_pri
(2) With using objects of property TA_TPRI
(3) With clearing an event flag for which two or more tasks waiting |
Fixed |
| Jul. 1, 2007 |
A Note on Using the Real-Time OS--M3T-MR30/4 V.4.00 Release 00--
for the M16C MCU Series |
(1) With using the ter_tsk service call |
Fixed |
| Nov. 16, 2006 |
Notes on Using the Real-Time OSes
M3T-MR308/4, -MR308 and M3T-MR30/4, -MR30 |
(1) With installing any product concerned to a directory whose path name contains spacecharacters
(2) With creating projects for real-time OSes on the High-performance Embedded
Workshop |
Fixed |
| Oct. 16, 2006 |
A Note on Using the C Compiler Packages--M3T-NC308WA and M3T-NC30WA--for the M16C MCU Family |
(1) With automatic generation of variable interrupt- and special page vector tables |
Fixed |
| Aug. 16, 2006 |
Notes on Using the Real-Time OSes M3T-MR308/4 and M3T-MR30/4 |
(1) On defining the interrupt handler
(2) On modifying the values concerning a fixed-size memory pool |
Fixed |
| June 5, 2006 |
The Real-Time OSes M3T-MR30K/4 and M3T-MR30S/4 Revised to V.4.00 Release 00 |
(1) V.3.30 Release 2 -> V.4.00 Release 00 |
-- |
The news that had been issued on and after release date of M3T-MR30 V.3.30 Release 2
The news that had been issued on and after release date of MR30 V.3.30 Release 1
The news that had been issued on and after release date of MR30 V.3.20 Release 1
The news that had been issued on and after release date of MR30 V.3.10 Release 1
The news that had been issued on and after release date of MR30 V.3.00 Release 1
|
 |