Skip to main content

Tool News

Real-Time OS HI1000/4 for the H8SX H8S family
See FAQs
See related news: Technical Update | High-performance Embedded Workshop | Real-Time OS Debugger

Issue Date Title Description Status on the
latest version
Nov. 16, 2008

The Real-Time OS--HI1000/4--for the H8SX and H8S MCU Families Revised to V.1.06 Release 00

V.1.05 Release 01 -> V.1.06 Release 00 --
Jun. 1, 2008

The Real-Time OS HI1000/4, Which Is Used for the H8SX and H8S MCU Families, Revised to V.1.05 Release 01

V.1.05 Release 00 -> V.1.05 Release 01 --
Jun. 1, 2008 A Note on Using the Real-Time OS HI1000/4, Which Is Used for the H8SX and H8S MCU Families (1) With clearing an event flag waited for by two or more tasks Fixed
Dec. 1, 2007 A Note on Using the Real-Time OS --HI1000/4 V.1.05 Release 00-- for the H8SX and H8S Families of MCUs (1) With selecting the product's release note among the Start menu of Windows (R) Fixed
Nov. 16, 2007

The Real-Time OS--HI1000/4--for the H8SX and H8S MCU Families Revised to V.1.05 Release 00

V.1.04 Release 00 -> V.1.05 Release 00 --
Nov. 16, 2007 Notes on Using the Real-Time OS--HI1000/4-- for the H8SX and H8S MCU Families (1) With issuing the chg_pri service call
(2)With issuing the ter_tsk service call
Fixed
Aug. 1, 2007 A Note on Using the Real-Time OS HI1000/4 V.1.04 Release 00 correction to the user's manuals --
Aug. 1, 2006 A Note on Using the Real-Time OS HI1000/4 V.1.04 Release 00 If you type a correct serial number into the Confirm Serial Number page displayed during execution of the update program shown below, an error arises and you will not be able to update the program. Fixed
Jul. 16, 2006

The Real-Time OS HI1000/4 Revised to V.1.04 Release 00

V.1.03 Release 00 -> V.1.04 Release 00 --
Jun 1, 2006 A Note on Using the Real-Time OSes for the SuperH and the H8SX Family of MCUs On dispatching an insignificant message when an update program is executed Not Fixed
Apr. 16, 2006 Corrections to the HI1000/4 User's Manual HI1000/4 user's manual (Document No. REJ10B0129-0100H) Not corrected
July 16, 2005 Notes on Using the Real-Time OSes HI7750/4, HI7700/4, HI7000/4, and HI1000/4 (1) On setting timer interrupt priority level (CFG_TIMINTLVL)
(2) On reading files not supported
Not Fixed


Real-Time OS HI2000/3 for the H8S family (Discontinued)
See FAQs
See related news: Technical Update | High-performance Embedded Workshop | Real-Time OS Debugger

Issue Date Title Description Status on the
latest version
Jun. 1, 2008 A Note on Using the Real-Time OSes HI2000/3 and HI8-2600 (Discontinued Products), Which Are Used for the H8S MCU Family With clearing an event flag waited for by two or more tasks No plan to fix
Nov. 1, 2005 A Note on Using the Real-Time OS HI2000/3 On calculating stack area size Not Fixed


Real-Time OS HI8-2600 for the H8S family (Discontinued)

Issue Date Title Description Status on the
latest version
Jun. 1, 2008 A Note on Using the Real-Time OSes HI2000/3 and HI8-2600 (Discontinued Products), Which Are Used for the H8S MCU Family With clearing an event flag waited for by two or more tasks No plan to fix




End of content

Back To Top