Skip to main content

Tool News

Real-time OS - M3T-MR100/4
Issue Time:
V.1.01 Release 00 | V.1.00 Release 00

The news that had been issued on and after release date of M3T-MR100/4 V.1.01 Release 00
Issue Date Title Description Status on the
Latest Version
Feb. 1, 2012 Notes on Using Real-Time OSes for R8C and M16C MCU Families (1) With task switching being delayed
(2) With dispatch disabled state
Not Fixed
May. 16, 2009 The Real-Time OS--M3T-MR100/4-- for the R32C/100 MCU Series Revised to V.1.01 Release 00 V.1.00 Release 00 -> V.1.01 Release 00 --

The news that had been issued on and after release date of M3T-MR100/4 V.1.00 Release 00
Issue Date Title Description Status on the
Latest Version
May 16, 2009 Notes on Using the Real-Time OS --M3T-MR100/4-- for the R32C/100 MCU Series (1) With using the timeout function
(2)With placing a fixed-length memory pool in a memory area
Fixed
Nov. 16, 2008 Corrections to the Manuals of Real-Time OSes M3T-MR100/4, M3T-MR308/4, and M3T-MR30/4 (1) Corrections in stack usage calculation methods Not Fixed
(Only M3T-MR100/4 has been fixed.)
Sep. 1, 2008 Notes on Using Real-Time OS M3T-MR100/4 V.1.00 Release 00 (1) With issuing the pol_sem and ipol_sem service calls
(2) With using the cyclic and alarm handlers
Fixed
Sep. 16, 2007 Real-Time OSes M3T-MR100K/4 and M3T-MR100S/4 V.1.00 Release 00 Published (1) M3T-MR100K/4 V.1.00 Release 00
(2) M3T-MR100S/4 V.1.00 Release 00
--




End of content

Back To Top