Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
C/C++ Compiler Package for SuperH family
(with simulator debbuger and Optimizing Linkage Editor)
See FAQs
See related news: Technical Update | High-performance Embedded Workshop | SQMlint | DeviceUpdater

Tool News for Ver.9
Issue Time:
V.9.02 R00 |
V.9.01 R01 | V.9.01 R00 |
V.9.00 R04A | V.9.00 R04 |V.9.00 R03 | V.9.00 R02 | V.9.00 R01 | V.9.00 R00 |
Tool News for Ver.8
Release information of previous versions: Ver.7 | Ver.6 | Ver.5

Tool News for Ver.9

In addition refer to the following News. The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.02 Release 00
Issue Date Title Description Status on the
Latest Version
Jul. 16, 2008 The Simulator Debugger for the SuperH RISC engine Family Revised to V.9.07.01 (1) V.9.02 Release 00 -> V.9.02 Release 01 --
Feb. 16, 2008 The C/C++ Compiler Package for the SuperH RISC engine MCU Family Revised to V.9.02 Release 00 (1) V.9.01 Release 01 -> V.9.02 Release 00 --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.01 Release 01
Issue Date Title Description Status on the
Latest Version
Feb. 16, 2008 Notes on Using the C/C++ Compiler Package for the SuperH RISC engine MCU Family (1) With using the Automatic Literal Pool Generation function
(2) With optimizing the program that contains instructions referencing literal pools using the linkage editor
Fixed
Sep. 16, 2007 A Note on Using the Simulator Debugger V.9.07.00 for the SuperH RISC engine MCU Family (1) With using the SH2A-FPU simulator Fixed
Sep. 1, 2007 The Simulator Debuggers for the SuperH RISC engine Family and the H8SX, H8S, and H8 Families of MCUs Revised (1) The simulator debugger for the SuperH RISC engine family V.9.07.00
(2) The simulator debugger for the H8SX, H8S, and H8 families V.5.06.00
--
Sep. 1, 2007 A Note on Using the C/C++ Compiler Package for the SuperH Family of MCUs (1) With using custom build phases with a specific name Not Fixed
Aug. 8, 2007 The C/C++ Compiler Package for the SuperH RISC engine Family of MCUs Revised to V.9.01 Release 01 (1) V.9.01 Release 00 -> V.9.01 Release 01 --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.01 Release 00
Issue Date Title Description Status on the
Latest Version
Jul. 16, 2007 A Note on Using the C/C++ Compiler Package V.9 for the SuperH RISC engine Family of MCUs (1) With multiplying a variable of type unsigned short and that of unsigned char Fixed
Apr. 1, 2007 The C/C++ Compiler Package for the SuperH RISC engine MCU Family Revised to V.9.01 Release 00 (1) V.9.00 Release 04A -> V.9.01 Release 00 --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.00 Release 04A
Issue Date Title Description Status on the
Latest Version
Mar. 1, 2007 Notes on Using the C/C++ Compiler Package V.9 for the SuperH RISC engine MCU Family (1) Problems in using the C/C++ compiler package V.9 for the SuperH RISC engine MCU family Fixed
Dec. 16, 2006 A Note on Using Debuggers for the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 MCU Families (1) With updating debuggers using the AutoUpdate Utility Not Fixed
Dec. 1, 2006 The Marketing of the Solaris and HP-UX Editions of the C/C++ Compiler Packages for the SuperH RISC engine; and the H8, H8S, and H8SX MCU Families Discontinued (1) We are discontinuing the marketing of the Solaris and
HP-UX editions.
--
Jul. 1, 2006 The Simulator Debuggers for the SuperH RISC Engine;and the H8SX, H8S, and H8 MCU Families Revised (1) The simulator debugger for the SuperH RISC engine V.9.06.00 --
Jun. 1, 2006 The C/C++ Compiler Package (Windows Edition) for the SuperH RISC Engine MCU Family Revised to V.9.00 Release 04A (1) V.9.00 Release 04 -> V.9.00 Release 04A (Only Windows Edition) --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.00 Release 04
Issue Date Title Description Status on the
Latest Version
Apr. 1, 2006 Notes on Using the C/C++ Compiler Package V.9 for the SuperH RISC Engine Family (1) Problem on Defining a Structure or Union after Declaring an Array of the Type of the Said Structure or Union
(2) On Assigning a Variable to a Parameter of a Function
(3) On Using a Function That Takes a Parameter Passed via the Stack
(4) On Assigning a 0 or 1 to a Volatile Variable in the True and False Statements of a Control Statement
Fixed
Apr. 1, 2006 The C/C++ Compiler Package for the SuperH RISC Engine Family Revised to V.9.00 Release 04 (1) V.9.00 Release 03 -> V.9.00 Release 04 --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.00 Release 03
Issue Date Title Description Status on the
Latest Version
Mar. 1, 2006 Notes on Using the C/C++ Compiler Package V.9 for the SuperH RISC Engine Family of MCUs (1) On Using Two or more Floating Constants
(2) On Performing Product-Sum Operations
(3) On Using do-while Statements
(4) On Using a Function Containing the Same Two or More Expressions
(5) On Using a Parameter within a Division or Remainder Operation
(6) On Using a Subtraction Expression within the Loop Body of an Iteration Statement
(7) On Declaring Pointer-Type Members within a Structure or Union Having an Alignment Number of 1
(8) On Performing an Operation Resulting in an Overflow
(9) On Using Special Loops
(10) On Using the opt_range Option
(11) On using the volatile_loop Option
(12) On Using the infinite_loop=0 Option
Fixed
Nov. 16, 2005 Notes on Using the C/C++ Compiler Package V.9 for the SuperH RISC Engine Family of MCUs (1) On calling a function that takes arguments passed via the stack
(2) On using a union that contains two or more members of the same structure or union type
Fixed
Nov. 1, 2005 A Note on Using the C/C++ Compiler Packages for the SuperH RISC Engine Family; and the H8, H8S, and H8SX Families of MCUs (1) On updating the compilers Fixed
Nov. 1, 2005 Notes on Using the C/C++ Compiler Package V.9 for the SuperH RISC Engine Family of MCUs (1) On defining a structure- or union-type array using the typedef specifier
(2) On making an assignment to a bit field of 1 bit wide that is a member of a structure- or union-type array
(3) On the referencing order of volatile-qualified variables
(4) On an initial value of a union containing a bit field as one of its members
(5) On a function taking a variable number of arguments
(6) On the controlling expression of a switch statement being of type long long or unsigned long long
(7) On Using Two or More Integer Constants
(8) On an Assignment to an Element of a volatile-Qualified Array
(9) On an Iteration Statement Having a volatile-Qualified Controlled Variable
(10) On Using Comma Operators in the Controlling Expression of an Iteration Statement
(11) On Using the Same Constant before and after a Function Call
Fixed
Sep. 1, 2005 A Note on Using the SuperH RISC Engine Family C/C++ Compiler Package V.9 (1) On displaying an HTML file after installing the product package Not Fixed
Aug. 1, 2005 The C/C++ Compiler Package for the SuperH RISC Engine Family Revised to V.9.00 Release 03 (1) V.9.00 Release 02 -> V.9.00 Release 03 The problem described in Section 2.3 in this news have been fixed

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.00 Release 02
Issue Date Title Description Status on the
Latest Version
Jun. 16, 2005 Notes on Using the C/C++ Compiler Package V.9 for the SuperH RISC Engine Family of MCUs (1) On Calling a Function That Takes an Argument Passed via the Stack
(2) On a Function That Contains Objects of Type double and float
(3) On the Return Value of a Function That Calls a strcpy() Function or Contains an Assignment Expression to a Member of a Packed Structure
(4) On Performing a Product-Sum Operation Containing a Pointer-Type Variable in a loop
(5) On Subtracting 1 from the Variable to Which the Evaluation Result of an Equality/Inequality Expression Is Assigned
(6) On a Result of a Residue Operation Where the Dividend and Divisor Are Constants of Powers of 2 and of Type long long
(7) On Dividing a Result of a Multiplication by an Integer Constant That is the Same as the Multiplicand or the Multiplier
(8) On Two Assignment Expressions to the Same Array Existing before an if Statement and in Its then Statement
Fixed
Jun. 7, 2005 A Note on Using the Evaluation Versions of Two C/C++ Compiler Packages (1) On using the evaluation versions of C/C++ compiler package V.9.00 Release 02 for SuperH and V.6.01 Release 00 for H8SX, H8S, and H8 Fixed in the latest evaluation versions of C/C++ compiler package
Jun. 1, 2005 The Update Programs of the C/C++ Compiler Packages for the SuperH RISC engine; and the H8, H8S, and H8SX Families Bug-Fixed (1) Update program shv9002u.exe, which updates the C/C++ compiler package for the SuperH RISC engine family to V.9.00 Release 02
(2) Update program h8v6100u.exe, which updates the C/C++ compiler package for the H8, H8S, and H8SX families to V.6.01 Release 00
--
May 16, 2005 A Note on Using the SuperH RISC Engine Simulator Debugger (1) On the number of execution cycles Fixed
May 16, 2005 A Note on Using the Update Programs of the C/C++ Compiler Packages for the SuperH RISC Engine Family and for the H8, H8S, and H8SX Families (1) On executing the update program Fixed in the latest update program
Apr. 16, 2005 A Note on Using the Simulator Debugger for the SuperH RISC Engine; and for the H8S Families and the H8/300 Series of MCUs--On Setting Access to Memory Resources (1) On setting access to memory resources Fixed
Apr. 16, 2005 A Note on Using the Optimizing Linkage Editor for the SuperH RISC Engine, H8, H8S, and H8SX Families of MCUs (1) On linkage list files generated by the optimizing linkage editor Fixed
Mar. 16, 2005 A Note on Using the Simulator Debugger for the SuperH RISC Engine Family--On Debugging Target Programs after Simulations of SH2A FPUs, SH-4A MCUs, and SH4AL DSPs (1) On debugging target programs after simulations of SH2A FPUs, SH-4A MCUs, and SH4AL DSPs. Not Fixed
Mar. 16, 2005 A Note on Using the Simulator Debuggers for the SuperH RISC Engine; and the H8, H8S, and H8SX Families (1) On using the simulator debugger for the SuperH RISC engine family and the one for the H8, H8S and H8SX families in the same host system. Fixed
Mar. 16, 2005 A Note on Using the C/C++ Compiler Packages for the SuperH RISC Engine; and the H8, H8S and H8SX Families (Windows Versions Only) (1) On executing the batch file for setting environmental variables Fixed
Mar. 1, 2005 Information on Renesas's Development Software Products Capable of Running on Windows XP Service Pack 2 -- --
Mar. 1, 2005 The C/C++ Compiler Package for the SuperH RISC Engine Family Revised to V.9.00 Release 02 (1) V.9.00 Release 01 -> V.9.00 Release 02 --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.00 Release 01
Issue Date Title Description Status on the
Latest Version
Jan. 16, 2005 The C/C++ Compiler Packages for the SuperH RISC engine family Revised to Their V.9.00 Release 01 (1) V.9.00 Release 00 -> V.9.00 Release 01 --

The news that had been issued on and after release date of C/C++ Compiler Package for SuperH family V.9.00 Release 00
Issue Date Title Description Status on the
Latest Version
Nov. 1, 2004 A Note on Using C/C++ Compiler Package V.9.00 Release 00 for the SuperH RISC engine Family Devices (1) On executing the RESBANK instruction in the SH2A-FPU Cycle Base Simulator (used for pipeline simulation) Fixed
Oct. 16, 2004 A Note on Using a C/C++ Compiler V.9.00 Release 00 for the SuperH RISC engine Family CPUs (1) On creating projects for the SH7206 microprocessor. Fixed
Oct. 1, 2004 The C/C++ Compiler Packages for the SuperH RISC engine family CPUs Upgraded to Their V.9.00 Release 00 (1) V.8.00 Release 04 -> V.9.00 Release 00 --

Tool News for Ver.8
Issue Date Title Description Status on the
Latest Version
Nov. 1, 2005 A Note on Using the C/C++ Compiler Packages for the SuperH RISC Engine Family; and the H8, H8S, and H8SX Families of MCUs (1) On updating the compilers Not Fixed
Jun. 1, 2005 The C/C++ Compiler Package for the SuperH RISC engine Family Revised to V.8.00 Release 05 V.8.00 Release 04 -> V.8.00 Release 05 --
Mar. 16, 2005 A Note on Using the C/C++ Compiler Packages for the SuperH RISC Engine; and the H8, H8S and H8SX Families (Windows Versions Only) (1) On executing the batch file for setting environmental variables Not Fixed
Feb. 16, 2005 A Note on Using the C/C++ Compiler Package V.8 for the SuperH RISC Engine Family (1) Eleven problems experienced in the compiler Fixed
-- Release Information of the C/C++ Compiler Package for the SuperH RISC engine Family V.8.00 Release 04 V.8.00 Release 03 -> V.8.00 Release 04 --
-- Release Information of the C/C++ Compiler Package for the SuperH RISC engine Family V.8.00 Release 03 V.8.00 Release 02 -> V.8.00 Release 03 --
-- Release Information of the C/C++ Compiler Package for the SuperH RISC engine Family V.8.00 Release 02 V.8.0.01 -> V.8.00 Release 02 --
-- Release Information of the C/C++ Compiler Package for the SuperH RISC engine Family V.8.0.01 V.8.0.01 --
Notes other than the above




© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal