| Issue Date |
Title |
Description |
| Apr. 16, 2009 |
Firmware of the SH7727
T-Engine Development Kit (R0P7727TH003TRK)
Updatable Free of Charge |
-- |
| Jul. 16, 2008 |
Information to Be Added to the User's Manual of the SH7780 T-Engine Development Kit |
-- |
| Jun. 1, 2008 |
The Ethernet Board Kit for T-Engine--R0P0000TH001ERK--Released,
Which is Connectable to the T-Engine Development Kit
for MCUs of the SuperH RISC engine Family
|
-- |
| Apr. 1, 2008 |
The T-Engine
Development Kit--R0P7760TH003TRKE-- for the SH7760
MCU, SuperH RISC engine Family Released |
-- |
| Mar. 16, 2008 |
The T-Engine
Development Kit--R0P7727TH003TRK-- for the SH7727
MCU, SuperH Family Released |
-- |
| Sep. 16, 2007 |
A Note
on Using the T-Engine Development Kit R0P7780TH001TRK
for the SH7780 MCU, SuperH Family |
"HI ApplicationEngine for T-Engine",
which is included with R0P7780TH001TRK, has been
revised from V2.0A to V2.0B |
| Feb. 1, 2006 |
A
T-Engine Development Kit R0P751RTH002TRK for the
SH7751R MCU (SuperH family) to Be Published |
-- |
| Aug. 12, 2005 |
A
Note on Using the T-Engine Development Kits --R0P751RTH001TRK,
R0P7760TH001TRK, and R0P7760TH002TRK |
If any USB device is
connected to or disconnected from your T-engine
development kit that has power supplied to it, a
power IC used in the 5-V power supply equipped with
the kit will be damaged, which causes the kit to
malfunction. |
| Aug. 1, 2005 |
The
µT-Engine Development Kit R0P7145TH001MRK
Released, Which Is Used for the SH7145 SuperH Family
MCU |
-- |