|
SuperH RISC engine C/C++ Compiler Package V.8.00 release03
Renesas C/C++ Compiler Package for SuperH RISC engine family V.8.00 release0x
was updated to V.8.00 release03.
This document list is the details of this upgrade.
| 1. High-performance Embedded Workshop (WindowsR version) |
1.1 Release of the restriction of High-performance Embedded Workshop V.3.01.02
We have corrected the following problems:
(1) Restriction of MAP Display
The "Linker section setting information" on a MAP window isn't
displayed.
(2) Restrictions of Virtual Desktop function
Don't open memory window on more than two window configurations of virtual
desktop function.
(3) Restriction of the "Include map file:" option
A link error might occur when "Include map file:" was
specified on the C/C++ tab of the Tools Options Dialog Box.
2.1 The new options
The following shows the options added to V.8.00.03.
- bss_order={declaration|definition}
- stuff[={bss|data|const}[,...]]
nostuff
2.2 Illegal Calculation of Quadratic Expression of Loop Induction Variable
We have fixed the problem of incorrectly calculating a quadratic expression
when loop induction variable was in this expression.
[Example]
int a[100];
void f() {
int i;
for (i=0;i<100;i++) {
a[i] = 3 * (i * i + 555 * i); /* illegally expanded to 3*i*i+555*i */
}
}
[Conditions]
This problem might occur when all of the following conditions were fulfilled.
(1) The optimize=1 option was specified.
(2) A loop existed.
(3) The loop of (2) had int/unsigned int/long/unsigned long-type loop induction
variable.
(4) A quadradic expression with the loop induction variable of (3) existed in
the loop of (2).
(5) The expression of (4) had the form of "m*(i*i+b*i)" (i:loop
induction variable m,b:variable or constant value).
2.3 Incorrect Removing of Sign/Zero Extension of a Constant Division (SHC-0001)
We have fixed the problem of removing the cast when a divisor and a dividend
were cast to the type of smaller size at a constant division and the result
of the division was assigned to a variable with a type after the cast.
[Example]
char c;
int i;
void func1() {
c = ((char)i / (char)2); /* a dividend was not cast to char-type */
}
void func2(){
c = ((char)i / (char)0x102); /* a divisor was not changed into 0x2 */
}
[Conditions]
This problem might occur when all of the following conditions were fulfilled.
(1) The optimize=1 option was specified.
(2) A constant division existed.
(3) A divisor and a dividend were cast to the type of smaller size at a constant
division of (2).
(4) Other than cpu=sh1 option and the division=cpu=inline option were specified,
or the divisor was a power of 2.
(5) The result of the division was assigned to a variable with a type after the
cast.
2.4 Incorrect replacement of loop induction variable (SHC-0003)
We have fixed the problem of incorrectly commonizing loop induction variables
when these variables existed and their type differed others in a loop.
[Example]
extern void g();
void func(unsigned int x) {
unsigned long i=3;
signed long k=3;
while (i<x) {
if (k<-3) { /* variable k was replaced illegally by variable i. */
break;
}
g();
--i;
--k;
}
}
[Conditions]
This problem might occur when all of the following conditions were fulfilled.
(1) The optimize=1 option was specified.
(2) A loop existed.
(3) The loop of (2) had a signed int type or signed long type loop induction
variable and an unsigned int type
or unsigned long type one.
(4) Initial values of the loop induction variables of (3) were constant value.
(5) Updating values of the loop induction variables of (3) were the same value.
| 3. Optimizing Linkage Editor |
3.1 Incorrect object due to specifying of delete unreferenced symbol optimization
The following problem were fixed.
When delete unreferenced symbol optimization was specified, a literal without
the symbol name was deleted illegally.
[Conditions]
This problem might occur when all of the following conditions were fulfilled.
(1) Object files were compiled with the goptimize option.
(2) A const variable which was not referred was in C source program.
(3) The string literal was used in C source program of (2).
(4) Some relocatable file including the object file of (2) was generated.
(5) The delete unreferenced symbol optimization (optimize=symbol_delete)
was valid when the relocatable file of (4) was
input.
3.2 Fixed internal error (L4001) with the strip option
The following problem with the linker version 8.00.04 was fixed.
An internal error (L4001) occurred when the strip option specified.
|