Boot RZ/V2H Evaluation Board Kit

This page describes how to boot the RZV2H Evaluation Board Kit (RZV2H EVK).

  1. Insert the microSD card to the Board.
    Note Use the microSD card slot SD1 on the Board as shown in the figure.

  2. Change DSW1 and DSW2 setting as shown in the figure.

  3. Connect the USB mouse and USB keyboard and USB camera via USB hub to the Board.
    Note There are USB 2.0 port and USB 3.0 port on RZ/V2H EVK.
    Please connect your USB camera to appropriate port according to its requirement.
    Here, USB camera is connected to USB 2.0 via USB hub.

  4. Connect an Ethernet cable between the Board and Linux Host PC.
  5. Connect the HDMI monitor to the Board.

  6. Connect the power cable to the Board.

  7. Turn the SW3 to ON.

  8. Turn the SW2 to ON to power on the Board.
v2h_boot
  1. After the boot-up, following screen will be displayed on HDMI monitor.
wayland
  1. Click the icon at the top-left corner to open the terminal.
wayland
  1. To communicate between your Linux Host PC and the Board via Ethernet, configure their respective IP addresses.
    • Linux PC:
      This uses the device name of the Ethernet interface "enp2s1" as an example and sets its IP address to 192.168.1.10..
      ifconfig enp2s1 192.168.1.10
    • Target board:
      Use eth0 and set its IP address to 192.168.1.11.
      ifconfig eth0 192.168.1.11