Boot RZ/V2L Evaluation Board Kit

This page describes how to boot the RZV2L Evaluation Board Kit (RZV2L EVK).

  1. Insert the microSD card to the Board.
    Note Use the microSD card slot CN3 as shown in the figure.

  2. Change SW1 and SW11 setting as shown in the figure.

  3. Connect an Ethernet cable between the board and Linux PC.
    Note Use the Ethernet connector Ethernet 0 as shown in the figure.
  4. Connect the USB mouse and USB keyboard via USB hub.

  5. Connect the Google Coral camera to the Board.

  6. Connect the HDMI monitor to the Board.

  7. Connect the power cable to the Board.

  8. Press power button for 1 second to turn on the board.
boot
  1. After the boot-up, following screen will be displayed on HDMI monitor.
wayland
  1. Click the icon at the top-left corner to open the terminal.
wayland
  1. To communicate between your Linux PC and the target board via Ethernet, configure their respective IP addresses.
    • Linux PC:
      This uses the device name of the Ethernet interface "enp2s1" as an example and sets its IP address to 192.168.1.10..
      ifconfig enp2s1 192.168.1.10
    • Target board:
      Use eth0 and set its IP address to 192.168.1.11.
      ifconfig eth0 192.168.1.11